2019-12-22 9:46 AM
Hi All,
I have a strange problem entering the Bootloader.
I need to send 0x7F twice to enter Bootloader.
Details:
I am working on a project where I need to program STM32H743xx MCU via UART pins. I was successful in programming STM32H743xx “Version Y�? via UART pins where I had to send 0x7F command once to enter the Bootloader.
Due to unavailability of the samples of ‘ Version Y ‘ , the supplier gave us ‘Version V’ samples and it’s strange that I need to send 0x7F command twice to enter the Bootloader.
Note: The PCB is custom made and the programming works fine for “Version Y�? and I am facing this problem for “Version V�?.
I would like to know if anybody is facing this problem and I would really appreciate if I can get any solution for this problem .
Thanks in advance.
2020-01-06 8:35 AM
Hello James,
Referring to AN2606, we find the following note for STM32H74x/5x devices: "To be able to connect to the bootloader USART1 using PB14/PB15 pins, you need to send two synchronization bytes."
Do you confirm that USART1 is used on your case?
Your description seems to be in contradiction with the one provided by @JYUNWEI wu on https://community.st.com/s/question/0D50X0000Bud5VTSQY.
Could you please precise: is one synchronization byte required for rev Y or rev V device?
Thanks,
Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-01-06 8:56 AM
Hai Amel,
Thank you very much for responding to my post.
Unfortunately the USART1 pins happens to be PB14/PB15 in my case. I had a formal discussion with ST FAE and tested both Nucleo board's with Version V & Y series MCU.
From the test's we concluded that only PB14/PB15 pins of Version V has this problem and rest other USART Bootloader pins of Version V & Y including PB14/PB15 pins of Version Y enters Bootloader successfully with one synchronization byte.
Thanks,
James
2020-01-06 9:09 AM
What you see as behavior using rev V is aligned with the note mentioned in AN2606.
I am checking internally: if it is not required to have 2 synchronization bytes with rev Y, this needs to be precised in AN2606.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-01-06 9:19 AM
Yes, I checked the revised version of AN2606 and they have mentioned about the synchronization bytes. But in the earlier version of AN2606 , this behavior wasn’t mentioned.
Yes that’s true this behavior has to be clearly mentioned in the document in order to avoid these confusions between versions
Thanks,
James
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.