2025-11-04 12:19 AM - last edited on 2025-11-06 3:36 AM by mƎALLEm
Post edited by ST moderator to be inline with the community rules for the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code.
HI ALL:
In my project, I use AWD1 to monitor ADC3_CHN1, then set the high and low threshold, it works very well.
However, when I switch to AWD2 and AWD3, there is no interrupt triggered, the setting codes are below:
The configuration for AWD1:
AnalogWDGConfig.WatchdogNumber = ADC_ANALOGWATCHDOG_1;
AnalogWDGConfig.WatchdogMode = ADC_ANALOGWATCHDOG_SINGLE_REG;
AnalogWDGConfig.Channel = ADC_CHANNEL_1; // output1 current
AnalogWDGConfig.HighThreshold = 800;
AnalogWDGConfig.LowThreshold = 500; /
AnalogWDGConfig.ITMode = DISABLE;
HAL_ADC_Stop(&hadc3);
if (HAL_ADC_AnalogWDGConfig(&hadc3, &AnalogWDGConfig) != HAL_OK) {
Error_Handler();
}
HAL_ADC_Start(&hadc3);
LL_ADC_ClearFlag_AWD1(hadc3.Instance);
LL_ADC_EnableIT_AWD1(hadc3.Instance);
The configuration of AWD2 and 3:
AnalogWDGConfig.WatchdogNumber = ADC_ANALOGWATCHDOG_2;
AnalogWDGConfig.WatchdogMode = ADC_ANALOGWATCHDOG_SINGLE_REG;
AnalogWDGConfig.Channel = ADC_CHANNEL_1; // output1 current
AnalogWDGConfig.HighThreshold = 800;
AnalogWDGConfig.LowThreshold = 500; /
AnalogWDGConfig.ITMode = DISABLE;
HAL_ADC_Stop(&hadc3);
if (HAL_ADC_AnalogWDGConfig(&hadc3, &AnalogWDGConfig) != HAL_OK) {
Error_Handler();
}
HAL_ADC_Start(&hadc3);
LL_ADC_ClearFlag_AWD2(hadc3.Instance);
LL_ADC_EnableIT_AWD2(hadc3.Instance);
The configurations are almost same, I wonder that whether the AWD2 and AWD3 support ADC3? If support adc3, Where is the problem with my code?
2025-11-05 4:51 PM
someone?
2025-11-06 3:17 AM
Contrary to watchdog 1, which can check only one channel (or all), watchdogs 2 and 3 can be set to check a set of channels, see Analog window watchdog subchapter of ADC chapter in RM. I wouldn't be surprised if this difference would mean a different API in Cube/HAL. I don't use Cube/HAL, but it's open source so you can check yourself.
I suggest to start with observing the ADC registers and comparing them between those two (working/non-working) cases; and then wind that back to how Cube sets those registes.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.