2023-06-05 3:52 AM
Both example and KB article depends on FreeRTOS.
Is there any real need to use FreeRTOS? In past I used LwIP without FreeRTOS just calling MX_LWIP_Process(). What do I need to do to get rid of FreeRTOS, is it enough to just disable it in STM32CubeMX and disable Ethernet Global Interript? I am afraid I run into some kind of Ethernet driver hidden problem.
2023-06-05 5:17 AM
If I remember correctly, after the last "rework" the HAL ETH driver should be used only with the interrupt. Polling variant of RX/TX functions (without _IT) has some issues.
2023-06-05 5:17 AM
Just tried to turn off "FreeRTOS": (FreeRTOS -> Interface: Disable) in STM32CubeMX.
Generated code doesn't even compile.
Is it even meant to run STM32H7 LwIp without FreeRTOS?
2023-06-05 5:49 AM
Pavel A. thank you.
I started with "just-worked" (ping worked ok) FreeRTOS + LwIP project
(CubeIDE 1.12.1, CubeMX Version: 6.8.1-RC4 Build: 20230419-1431)
void sys_lock_tcpip_core(void){}
void sys_unlock_tcpip_core(void){}
void sys_check_core_locking(void){}
void sys_mark_tcpip_thread(void){}
3) Added MX_LWIP_Process() in main loop...
No ping in result. For now.
Compared both codebases, looked for "ETH_CODE"... nothing suspicious... seems need to double-check entire Piranha list (?)...
Year ago I just ignored "modern reworked drivers" for Stm32F4 using CubeMX 6.4.0 with STM32Cube_FW_F4_V1.26.2
it all worked ok.
In which version for H7 eth HAL driver breaked?
2023-06-05 6:06 AM
Yes, LwIP can be used without FreeRTOS and in Cube firmware packages there are ETH examples without FreeRTOS.
2023-06-05 7:08 AM
Unfortunately all new STM32H7 examples at https://github.com/stm32-hotspot/STM32H7-LwIP-Examples/ use FreeRTOS.
The first H7 library release after "rework" is 1.10.0.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.