2025-07-15 10:00 PM - last edited on 2025-08-27 3:50 AM by Amel NASRI
Hi Team,
I made a custom board using STM32F769BIT microcontroller using with the DP83867 PHY in MII mode, but I am not able to ping it. What could be the possible reasons?
I did Memory configurations for TxDecrip, RxDecrip, LwipHeap like this.
.lwip_sec (NOLOAD) :
. = ABSOLUTE(0x2007C000);
*(.RxDecripSection)
. = ABSOLUTE(0x2007C0A0);
*(.TxDecripSection)
. = ABSOLUTE(0x2007C140);
*(.LwIPHeap)
also my SRAM configuration is like this_
MEMORY
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 496K
SRAM2 (xrw) : ORIGIN = 0x2007C000, LENGTH = 16K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 2048K
I am using the 10pin STM32 debugger, but I am not able to see the stack usage there, when I press the debug button.
Is it due to code or due to the debugger? For this should I need the 20pin debugger?
Thanks,
Sayan Das
2025-08-25 2:10 AM
Hello @Sayan,
I suggest you provide the current status of your debugging process so I can assist you and help speed it up. This way, you can get your solution working in a shorter time.
Best regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.