2025-07-15 10:00 PM - last edited on 2025-08-27 3:50 AM by Amel NASRI
Hi Team,
I made a custom board using STM32F769BIT microcontroller using with the DP83867 PHY in MII mode, but I am not able to ping it. What could be the possible reasons?
I did Memory configurations for TxDecrip, RxDecrip, LwipHeap like this.
.lwip_sec (NOLOAD) :
. = ABSOLUTE(0x2007C000);
*(.RxDecripSection)
. = ABSOLUTE(0x2007C0A0);
*(.TxDecripSection)
. = ABSOLUTE(0x2007C140);
*(.LwIPHeap)
also my SRAM configuration is like this_
MEMORY
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 496K
SRAM2 (xrw) : ORIGIN = 0x2007C000, LENGTH = 16K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 2048K
I am using the 10pin STM32 debugger, but I am not able to see the stack usage there, when I press the debug button.
Is it due to code or due to the debugger? For this should I need the 20pin debugger?
Thanks,
Sayan Das
2025-07-16 12:02 AM
Does you code work on a validated board, like a Nucleo one (obvious, with legacy PY interface)?
This should tell if is a PHY problem or a coding problem.
2025-07-16 1:44 AM
I don't have nucleo board. Is there any way to debug?
2025-07-16 1:52 AM - edited 2025-07-16 1:53 AM
A) your board is defective
B) your code is wrong
which one is your case?
Get one board 100% tested and test your code - later you can test your hw !!
2025-07-16 1:58 AM
Hello @Sayan, and Welcome to the community!
To maximize your chances of finding a solution, please refer to How to write your question to maximize your chances to find a solution for best practices.
In particular, please include the following details in your post:
Providing this information helps the community assist you more effectively.
Best regards,
2025-07-16 2:07 AM - edited 2025-07-16 2:14 AM
As @STackPointer64 said, more info is needed.
You haven't said what IP stack you're using - they usually have options for diagnostic output to help debug...
@Sayan wrote:I am using the 10pin STM32 debugger
But have you correctly wired it?
That's why showing your schematic is essential!
How have you validated your DP83867 design? Previous discussions relating to DP83867:
PS:
Have you checked-out TI's Product Page for the DP83867 - I can see a couple of debugging/troubleshooting guides there:
https://www.ti.com/product/DP83867E#tech-docs
https://www.ti.com/product/DP83867E#software-development
2025-07-24 10:21 PM
2025-07-24 11:17 PM
I am describing my settings here - in ETH, my mode is MII. In the Eth parameter settings, Tx and RX Descriptor Lenth is 4 and Rx Descriptor address is 0x2007c000, and Tx Descriptor address is 0x2007c0a0. The RX mode is Interrupt.
I have varrified the GPIOs. The GPIO connection is fine.
In the NVIC interupt table the Ethernet Global Interrupt is checked, but ethernet wake-up interrupt through EXTI line 19 is not checked.
In the FREERTOS, CMSIS_V1 interface is selected. Else others are as it is.
In LWIP Settings, in general settings, LWIP_DHCP is disabled and I put the static IP. IP_Address is 172.16.000.100, Netmask_Address is 255.255.000.000 and gateway_address is 172.16.0.1. I incresead the heap memory size to 16000 bytes and the address of LWIP_RAM_HEAP_POINTER is 0x2007c140. From the checksum option the CHECKSUM_BY_HARDWARE is enabled. The only platform option was DP83848. Other things are unchanged.
After that I generate the code.
This is the configuration.
Is everything fine?
2025-07-24 11:35 PM - last edited on 2025-07-25 2:14 AM by Andrew Neil
My main.c looks like this.
#include "main.h"
#include "cmsis_os.h"
#include "lwip.h"
UART_HandleTypeDef huart6;
osThreadId defaultTaskHandle;
void SystemClock_Config(void);
static void MPU_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART6_UART_Init(void);
void StartDefaultTask(void const * argument);
int main(void)
{
MPU_Config();
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_USART6_UART_Init();
osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 256);
defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);
osKernelStart();
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
HAL_PWR_EnableBkUpAccess();
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 8;
RCC_OscInitStruct.PLL.PLLN = 216;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
if (HAL_PWREx_EnableOverDrive() != HAL_OK)
{
Error_Handler();
}
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_7) != HAL_OK)
{
Error_Handler();
}
}
static void MX_USART6_UART_Init(void)
{
huart6.Instance = USART6;
huart6.Init.BaudRate = 115200;
huart6.Init.WordLength = UART_WORDLENGTH_8B;
huart6.Init.StopBits = UART_STOPBITS_1;
huart6.Init.Parity = UART_PARITY_NONE;
huart6.Init.Mode = UART_MODE_TX_RX;
huart6.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart6.Init.OverSampling = UART_OVERSAMPLING_16;
huart6.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart6.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart6) != HAL_OK)
{
Error_Handler();
}
}
static void MX_GPIO_Init(void)
{
__HAL_RCC_GPIOE_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOI_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOG_CLK_ENABLE();
}
void StartDefaultTask(void const * argument)
{
MX_LWIP_Init();
for(;;)
{
osDelay(1);
}
}
void MPU_Config(void)
{
MPU_Region_InitTypeDef MPU_InitStruct = {0};
HAL_MPU_Disable();
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER0;
MPU_InitStruct.BaseAddress = 0x0;
MPU_InitStruct.Size = MPU_REGION_SIZE_4GB;
MPU_InitStruct.SubRegionDisable = 0x87;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.AccessPermission = MPU_REGION_NO_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
}
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
if (htim->Instance == TIM6)
{
HAL_IncTick();
}
}
void Error_Handler(void)
{
__disable_irq();
while (1)
{
}
}
#ifdef USE_FULL_ASSERT
void assert_failed(uint8_t *file, uint32_t line)
{
}
#endif /* USE_FULL_ASSERT */Edited to apply source code formatting - please see How to insert source code for future reference.
See also: How to write your question to maximize your chances to find a solution, linked earlier.
2025-07-25 2:49 AM
@mbarg.1 wrote:A) your board is defective
B) your code is wrong
Or both!
@Sayan Hence the importance of starting on a known-good board - such as a Nucleo.
The advantage of using an ST board in particular is that it will be well-known by people here.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.