2014-12-15 9:46 AM
Hello,
is there a possible way to access the Bootloader-Mode after a System-Reset without the use of the BOOT0 and BOOT1 Pins? For example, write a value to a backup register and after a reset this backup register is read and the STM32F4Discovery jumps to the Bootloader. kind regards #stm32f4 #discovery #stm32f4-bootloader2014-12-15 9:52 AM
I've covered this at least a dozen times on the forum, please search/google.
2014-12-15 11:02 AM
I am googleing since two weeks but the only way i found was a very bad explained youtube video how to get to the bootloader from the user application.
In this case i must reconfigure the clocks, disable the interrupts and so on. I am looking for a faster way to access the bootloader via a soft-reset. Can you give me some links for that theme?2014-12-15 12:25 PM
I am googleing since two weeks but... Got to really work on those searching skills then.
https://community.st.com/0D50X00009XkhAzSAJ
https://community.st.com/0D50X00009Xka1fSAB
https://community.st.com/0D50X00009Xkh7wSAB
https://community.st.com/0D50X00009XkhgYSAR
https://community.st.com/0D50X00009XkbZhSAJ
https://community.st.com/0D50X00009XkYIbSAN
Edit:Removed DEADLINKs, original post from 14-Dec-2014
2014-12-16 12:54 AM
Hi Clive,
thanks a lot for sharing this links! I am not a real Software Engineer but i have to solve the problem to access the bootloader. Can you tell me how i have to implement this part of assembler code that it works after a reset?Reboot_Loader PROC
EXPORT Reboot_Loader
LDR R0, =0x40023844 ; RCC_APB2ENR
LDR R1, =0x00004000 ; ENABLE SYSCFG CLOCK
STR R1, [R0, #0]
LDR R0, =0x40013800 ; SYSCFG_MEMRMP
LDR R1, =0x00000001 ; MAP ROM AT ZERO
STR R1, [R0, #0]
LDR R0, =0x1FFF0000 ; ROM BASE
LDR SP,[R0, #0] ; SP @ +0
LDR R0,[R0, #4] ; PC @ +4
BX R0
ENDP ; sourcer32@gmail.com
Thanks again for your help, you get me out of trouble.
2014-12-16 7:36 AM
I am not a real Software Engineer...
Me neither, my degree is in Electrical and Electronic Engineering Quick blind mash of the existing example code; Keil based example - Reset into boot loader - sourcer32@gmail.com
; From C
; extern void SystemReset(void);
; *((unsigned long *)0x2001FFF0) = 0xDEADBEEF; // Write a scratch location at end of RAM (or wherever)
; SystemReset();
Reset_Handler PROC
EXPORT Reset_Handler
IMPORT __main
;...
LDR R0, =0x2001FFF0 ; Address for RAM signature
LDR R1, =0xDEADBEEF
LDR R2, [R0, #0] ; Read current
STR R0, [R0, #0] ; Invalidate
CMP R2, R1
BEQ Reboot_Loader
; Add other choices
;...
; Normal startup path
LDR R0, =SystemInit
BLX R0
LDR R0, =__main
BX R0
ENDP
;...
; Vector into System Loader
Reboot_Loader PROC
EXPORT Reboot_Loader
LDR R0, =0x40023844 ; RCC_APB2ENR
LDR R1, =0x00004000 ; ENABLE SYSCFG CLOCK
STR R1, [R0, #0]
LDR R0, =0x40013800 ; SYSCFG_MEMRMP
LDR R1, =0x00000001 ; MAP ROM AT ZERO
STR R1, [R0, #0]
LDR R0, =0x1FFF0000 ; ROM BASE
LDR SP,[R0, #0] ; SP @ +0
LDR R0,[R0, #4] ; PC @ +4
BX R0
ENDP ; sourcer32@gmail.com
SystemReset PROC
EXPORT SystemReset
ldr r1, =0xE000ED0C ; NVIC Application Interrupt and Controller
ldr r0, =0x05FA0004 ; Magic
str r0, [r1, #0] ; Reset
b .
ENDP
;...
2014-12-18 12:52 AM
Well, it seems that i can access the Bootloader with the following codes:
in the s file: Reset_Handler PROC EXPORT Reset_Handler [WEAK] IMPORT __main LDR R0, =0x2001FFF0 LDR R1, =0xDEADBEEF LDR R2, [R0, #0] STR R0, [R0, #0] ; Invalidate CMP R2, R1 BEQ Reboot_Loader LDR R0, =__main BX R0 ENDP Reboot_Loader PROC EXPORT Reboot_Loader LDR R0, =0x1FFF0000 LDR SP, [R0, #0] LDR R0, [R0, #4] BX R0 ENDP Calling it in the C File: #include ''misc.h'' void blac(void){ NVIC_InitTypeDef NVIC_InitStructure; *((unsigned long *)0x2001FFF0) = 0xDEADBEEF; // 128kB STM32F407 NVIC_SystemReset(); } When i call it the STM32 BOOTLOADER Device appears in the Devices Manager. Now i am trying to communicate with the STM32F4Discovery Bootloader via can. I hope i am on the right way. If not, please leave a comment. Kind regards and thank you very very much clive1!2018-08-09 5:39 PM
Apparently not able to edit my own post to fix the dog's breakfast that the port to the new forum created. Should work for F2 and F4 parts to switch into DFU/USART System Loader ROM
The following C and Assembler provide a means to execute the boot ROM of STM32F2 and F4 parts. It sets a value in RAM and then resets, the reset catches this value and remaps the ROM and jumps into it.
startup.s
; Keil based example - Reset into boot loader - sourcer32@gmail.com
; From C
; extern void SystemReset(void);
; *((unsigned long *)0x2001FFF0) = 0xDEADBEEF; // Write a scratch location at end of RAM (or wherever)
; SystemReset(); // or NVIC_SystemReset();
Reset_Handler PROC
EXPORT Reset_Handler
IMPORT __main
;...
LDR R0, =0x2001FFF0 ; Address for RAM signature
LDR R1, =0xDEADBEEF
LDR R2, [R0, #0] ; Read current
STR R0, [R0, #0] ; Invalidate
CMP R2, R1
BEQ Reboot_Loader
; Add other choices
;...
; Normal startup path
LDR R0, =SystemInit
BLX R0
LDR R0, =__main
BX R0
ENDP
;...
; Vector into System Loader
Reboot_Loader PROC
EXPORT Reboot_Loader
LDR R0, =0x40023844 ; RCC_APB2ENR
LDR R1, =0x00004000 ; ENABLE SYSCFG CLOCK
STR R1, [R0, #0]
LDR R0, =0x40013800 ; SYSCFG_MEMRMP
LDR R1, =0x00000001 ; MAP ROM AT ZERO
STR R1, [R0, #0]
LDR R0, =0x1FFF0000 ; ROM BASE
LDR SP,[R0, #0] ; SP @ +0
LDR R0,[R0, #4] ; PC @ +4
BX R0
ENDP ; sourcer32@gmail.com
SystemReset PROC
EXPORT SystemReset
ldr r1, =0xE000ED0C ; NVIC Application Interrupt and Controller
ldr r0, =0x05FA0004 ; Magic
str r0, [r1, #0] ; Reset
b .
ENDP
;...Now accepting PayPal, Venmo and Amazon Gift Cards..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.