2018-02-06 1:14 PM
Hi,
I'm currently working on a project based on STM32 and I need a WiFi connection in order to send information to a mobile app.
My project can be divided in 2 parts : a prototype with 2 PCBs and then an industrial PCB production.
First, I tough use
coupled with this module wifihttp://www.st.com/stm32f4dis-expansion/
.For the second part, I already seen the
as a solution to produce in SMD.I have just one fear : There isn't library to use STM32F4DIS-WIFI. Is it so possible to use the one of SPWF01SA ? Are the SPWF01SA and STM32F4DIS-WIFI compatible for coding ?If you have a better idea, I'm at the beginning of the project and this is so possible to change of solution !Thanks a lot#wifi-spwf01sa #stm32f4discovery #wifi-module2018-02-06 6:29 PM
The STM32F4DIS-WIFI is very dated. The SPWF01SA has been superseded by the
http://www.st.com/en/wireless-connectivity/spwf04sa.html
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.