2017-06-07 5:09 AM
Hello all,
In the process of learning Microcontroller programming, I have taken up a project where in I have mounted a cellular modem to my Discover kit and passing commands(Pre Programmed) to modem with MCU. Now, I want to transfer a file with large size ranging 10MB+, as flash memory is limited to 2MB , I have created a uint16_t array of ST_logo converted image which looks like { 0xFFFF, 0xFFFF, ....etc. } (Hexadecimal)�and transmitted with UART to Modem which works fine.
Now, when I want to transfer the file more than 10MB, what are the possibilities? I have checked USB-OTG is a support for this Discovery kit, but I couldn't find any examples which could help me. My idea is to Place a file of 10MB or more in a USB stick, start reading from MCU and at the same time transmitting to Modem. Will this work? If so, how to implement. Any small example would help me a lot. Thanks in advance.
P.S: I have already worked with CubeMX,System workbench for STM32 and developed SMS applications, like I can send SMS with modem and MCU kit.
Regards,
Munna
#rx #stm32f429zit6-discovery #usb-otg-file-tx #transmittingWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.