2023-09-09 5:27 AM
Hello,
I'm trying to use FatFS with both USB HOST MSC class and SDIO.
FatFS always tries to access the SD card whatever the drive number used in f_mount.
May be I'm wrong with the path I use to access the devices : "0" for SD card, "1" for USB.
Any help will be welcome.
Solved! Go to Solution.
2023-09-09 6:44 AM
Issue is solved.
I stepped into f_mount and found thaht the path was missing the ":" i.e. path must be "0:" or "1:" not bjust "0" or "1".
Thanks for the answer :)
2023-09-09 6:11 AM
2023-09-09 6:44 AM
Issue is solved.
I stepped into f_mount and found thaht the path was missing the ":" i.e. path must be "0:" or "1:" not bjust "0" or "1".
Thanks for the answer :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.