2020-06-08 6:07 AM
I m using LwIP+FreeRTOS (STM32Cube FW library for STM32f4xx 1.25.0).
I use the Ethernet to send TCP and UDP packets. Everything works fine: I have HTTP working, I can join Multicast groups (IGMP), I can send UDP packets on regular addresses.
But I can't send UDP packets on a multicast address. IGMP membership queries are fine but no UDP communication.
I traced it back down to the DMA transfer where I wasn't able to find anything wrong but the packet is never sent according to Wireshark from another machine.
Is there a specific setting to enable that or I am missing something ?
NB : The code is based on the demo project from the library with the IGMP settings advised on this support forum.
2021-04-25 7:36 PM
Dear, BCall.1,
Did you solve the problem.
I have a same problem.
--- < source code > ---
netbuf_alloc(tx_buf, len);
pbuf_take(tx_buf->p, (const void *)ptr, len);
err = netconn_sendto(conn, tx_buf, (const ip_addr_t *)&dstIP, dstPORT); // Destination : 239.192.0.2, Port 60002
----------------------------------
return value is ERR_OK.
but, data output is nothing.
At the same time, it transmits UDP,, it is output normally. (Destination : 192.168.10.10, Port 5100)
Please, let me know the your status!
Best regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.