2018-12-28 5:51 AM
Hi,
I am using stm32f429 based eval board with mynewt OS which has lwip stack integrated.
I am facing a problem when i connect device to the LAN (around hundred hosts connected on the same LAN) , as follows.
Performing the ping continuously , successfull for some 10 minutes, after that ping fails saying "Destination unreachable". I am expecting that the device disconnected from the LAN and not able to reconnect to the LAN.
But this doesn't happens if i connect the stm32f429 device and PC to a separate router. Ping succeeded continuously without interruptions for > 2 hours untill i disconnect them.
From this i can say that due heavy traffic device got disconnected to the network, but not able to reconnect.
Any idea that how can i make the device automatically reconnect to the network ? What could be the problem ?
2020-06-05 1:39 AM
Hi,
I also have the problem you mentioned. Did you find any solution before?
2020-06-10 4:37 PM
Check the PHY link speed and duplex bits and take a look on this:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.