2014-11-25 11:09 PM
STM32F411RCTx, LQFP64
When using STM32CubeMX Ver4.4 to generate USB Device only code for CDC class, initialization is fine but cannot connect to PC (host).The STM32CubeMX generated code also has same problem as MDK-ARM 5.xx USB device driver. It could be resulting from ''power saving mode
'' or ''VBus voltage sensing
'' for STM32F411.For example,*****************************************************************
* @file : usbd_conf.c * @date : 24/11/2014 18:53:54 * @version : v1.0_Cube * @brief : This file implements the board support package for the USB device library*********************************************************************** USBD_StatusTypeDef USBD_LL_Init (USBD_HandleTypeDef *pdev) { /* Init USB_IP */ if (pdev->id == DEVICE_FS) { /* Link The driver to the stack */ hpcd_USB_OTG_FS.pData = pdev; pdev->pData = &hpcd_USB_OTG_FS; hpcd_USB_OTG_FS.Instance = USB_OTG_FS; hpcd_USB_OTG_FS.Init.dev_endpoints = 7; hpcd_USB_OTG_FS.Init.speed = PCD_SPEED_FULL; hpcd_USB_OTG_FS.Init.dma_enable = DISABLE; hpcd_USB_OTG_FS.Init.ep0_mps = DEP0CTL_MPS_64; hpcd_USB_OTG_FS.Init.phy_itface = PCD_PHY_EMBEDDED; hpcd_USB_OTG_FS.Init.Sof_enable = DISABLE;//hpcd_USB_OTG_FS.Init.low_power_enable = ENABLE;
hpcd_USB_OTG_FS.Init.low_power_enable = DISABLE; hpcd_USB_OTG_FS.Init.vbus_sensing_enable = DISABLE; hpcd_USB_OTG_FS.Init.use_dedicated_ep1 = DISABLE; hpcd_USB_OTG_FS.Init.use_external_vbus = DISABLE; HAL_PCD_Init(&hpcd_USB_OTG_FS); HAL_PCD_SetRxFiFo(&hpcd_USB_OTG_FS, 0x80); HAL_PCD_SetTxFiFo(&hpcd_USB_OTG_FS, 0, 0x40); HAL_PCD_SetTxFiFo(&hpcd_USB_OTG_FS, 1, 0x80); } return USBD_OK; }At line 268 of usbd_conf.c, disable the ''low_power_enable'' flag then USB device can work fine...I have no idea what is going on USB driver for STM32F411 body. Please address me if you have similar issue.Thank you! #usb-cdc #stm32f4112014-12-07 5:03 AM
I ran into the same problem with STM32F407VG. Disabling the low power mode helped me a bit too. The COM port is now registered, but the device manager is reporting ''{Operation Failed} The requested operation was unsuccessful. C0000001''. Any further info would be appreciated.
Regards,Matija2014-12-07 6:35 AM
Found my problem! The heap was too small (0x0200). After I increased it, everything started working.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.