2019-03-14 9:34 PM
We have purchased stm32f407vg discovery board plus Base board from element 14 with ethernet and other peripherals. We observe ethernet works but mdio communication is not working as expected. We are not seeing MDC and MDIO signals and Ref clk clock has an offset of 1.45 volts with 200 mV 50 Mhz signal
2019-03-15 7:05 AM
Hello,
Maybe you should check pins configuration.
Is this issue faced when used the Cube example?
Kind Regards,
Imen.
2019-03-15 6:43 PM
/* Ethernet pins configuration ************************************************/
/*
ETH_MDIO --------------> PA2
ETH_MDC ---------------> PC1
ETH_RMII_REF_CLK-------> PA1
ETH_RMII_CRS_DV -------> PA7
ETH_MII_RX_ER -------> PB10
ETH_RMII_RXD0 -------> PC4
ETH_RMII_RXD1 -------> PC5
ETH_RMII_TX_EN -------> PB11
ETH_RMII_TXD0 -------> PB12
ETH_RMII_TXD1 -------> PB13
ETH_RST_PIN -------> PE2
*/
/* Configure the PHY RST pin */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOE, &GPIO_InitStructure);
GPIO_ResetBits(GPIOE, GPIO_Pin_2);
for (i = 0; i < 20000; i++);
/* Configure PA1,PA2 and PA7 */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_7;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource1, GPIO_AF_ETH);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_ETH);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_ETH);
/* Configure PB10,PB11,PB12 and PB13 */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_12 | GPIO_Pin_13;
GPIO_Init(GPIOB, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource10, GPIO_AF_ETH);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource11, GPIO_AF_ETH);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource12, GPIO_AF_ETH);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource13, GPIO_AF_ETH);
/* Configure PC1, PC4 and PC5 */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 | GPIO_Pin_4 | GPIO_Pin_5;
GPIO_Init(GPIOC, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource1, GPIO_AF_ETH);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource4, GPIO_AF_ETH);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource5, GPIO_AF_ETH);
GPIO_SetBits(GPIOE, GPIO_Pin_2);
for (i = 0; i < 20000; i++);
The above code is used for initialization of the ethernet module. We are using
the ethernet BSP driver which may along with Base board (Element 14).
The ethernet communication is working with default setting, but registers
are always reading 0xffff. We do not see any activity on the mdio/mdc pins.
2019-03-27 7:23 AM
Hi,
What is the PHY address ? Is your ethernet PHY enabled and how is PHY clocked, exactly?
Regards
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.