2017-11-19 4:50 AM
I created a project by CubeMx and enabled Ethernet in RMII mode plus LWIP.
I am trying to send UDP packet with this code :
void udpAppi_sendPacket(void)
{ip_addr_t client1IpAddr;
IP4_ADDR(&client1IpAddr , 192 , 168 ,0,2); ethTxBuffer_p = pbuf_alloc(PBUF_RAW_TX , bufferSize , PBUF_RAM); memcpy(ethTxBuffer_p ->payload , fakeBuffer , bufferSize); status = udp_sendto(udpPcb1_p ,ethTxBuffer_p ,&client1IpAddr , 5222); pbuf_free(ethTxBuffer_p);}
and in the main function :
while (1)
{HAL_Delay(100);
udpAppi_sendPacket(); ethernetif_input(&gnetif); sys_check_timeouts();}
every thing is Ok until packet length is smaller than MTU size which is 1500 byte. when i increased the packet size to 1600 no packet was sent.
then i increased MEM_SIZE from 1600 to 10240 and now i can see the fragmented packets with Wireshark(network sniffer) in my PC but the packets checksum are incorrect, so they will be dropped.
is there any parameter that should be changed? i dont think that this is the LWIP 's bug.
i am working on it more than a week.please help me.
any suggestion would be appreciated.
thanks in advance
#raw-lwip #udp #etherent #lwip* #stme32-cube2017-11-20 1:34 AM
You may want to ask general lwip questions in
https://lists.nongnu.org/mailman/listinfo/lwip-users
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.