2022-11-29 5:54 PM
Hi.
I used USB_OTG_FS as Audio Device Class on STM32F407-discovery.
I connected PC and STM32F407-discovery with USB device.
When I played music, sometimes sound is not occurred on STM32F407-discovery.
I found that epnum in USBD_LL_DataOutStage is always 0 if sound is not occurred. (It is not 0 if sound is occurred.)
But I don't know what epnum is and how it is changed.
Could somebody help me how to fix this issue?
Firmware : STM32Cube_FW_F4_V1.27.0
===================================================================
USBD_StatusTypeDef USBD_LL_DataOutStage(USBD_HandleTypeDef *pdev,
uint8_t epnum, uint8_t *pdata)
{
USBD_EndpointTypeDef *pep;
USBD_StatusTypeDef ret = USBD_OK;
uint8_t idx;
printf("USBD_LL_DataOutStage %d\r\n",epnum);
if (epnum == 0U)
{
pep = &pdev->ep_out[0];
if (pdev->ep0_state == USBD_EP0_DATA_OUT)
{
if (pep->rem_length > pep->maxpacket)
{
pep->rem_length -= pep->maxpacket;
(void)USBD_CtlContinueRx(pdev, pdata, MIN(pep->rem_length, pep->maxpacket));
}
else
{
/* Find the class ID relative to the current request */
switch (pdev->request.bmRequest & 0x1FU)
{
case USB_REQ_RECIPIENT_DEVICE:
/* Device requests must be managed by the first instantiated class
(or duplicated by all classes for simplicity) */
idx = 0U;
break;
case USB_REQ_RECIPIENT_INTERFACE:
idx = USBD_CoreFindIF(pdev, LOBYTE(pdev->request.wIndex));
break;
case USB_REQ_RECIPIENT_ENDPOINT:
idx = USBD_CoreFindEP(pdev, LOBYTE(pdev->request.wIndex));
break;
default:
/* Back to the first class in case of doubt */
idx = 0U;
break;
}
if (idx < USBD_MAX_SUPPORTED_CLASS)
{
/* Setup the class ID and route the request to the relative class function */
if (pdev->dev_state == USBD_STATE_CONFIGURED)
{
if (pdev->pClass[idx]->EP0_RxReady != NULL)
{
pdev->classId = idx;
pdev->pClass[idx]->EP0_RxReady(pdev);
}
}
}
(void)USBD_CtlSendStatus(pdev);
}
}
else
{
#if 0
if (pdev->ep0_state == USBD_EP0_STATUS_OUT)
{
/*
* STATUS PHASE completed, update ep0_state to idle
*/
pdev->ep0_state = USBD_EP0_IDLE;
(void)USBD_LL_StallEP(pdev, 0U);
}
#endif
}
}
else
{
/* Get the class index relative to this interface */
idx = USBD_CoreFindEP(pdev, (epnum & 0x7FU));
if (((uint16_t)idx != 0xFFU) && (idx < USBD_MAX_SUPPORTED_CLASS))
{
/* Call the class data out function to manage the request */
if (pdev->dev_state == USBD_STATE_CONFIGURED)
{
if (pdev->pClass[idx]->DataOut != NULL)
{
pdev->classId = idx;
ret = (USBD_StatusTypeDef)pdev->pClass[idx]->DataOut(pdev, epnum);
}
}
if (ret != USBD_OK)
{
return ret;
}
}
}
return USBD_OK;
}
===================================================================
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.