2020-01-27 9:49 PM
Hi,
try debug with SWV my simple blinky programm but it dosn't work correct.
I use a simple USB-cable (ST-LINK)to connect with my Win10 PC. STMCube is updated to 1.2.1
Here the code of the _write function:
int _write(int file, char *ptr, int len)
{
/* Implement your write code here, this is used by puts and printf for example */
int i=0;
for(i=0 ; i<len ; i++)
ITM_SendChar((*ptr++));
return len;
}So i've a few questions ...
A) At Debug configuration: I found several values for core Clock and SWOClock.
I think coreclock is the same value like my controller but were i find the correct value for SWO-clock?
B) Data trace: which is the correct addres and where i can find it?
Currently i can read the variable (counter i of a "for"-loop) via "view memeory".
But it dosn't work at runtime ... i have to pasue and then values of the memory-view will updated. If i click on "play"-Button values are frezzed -> ...pause -> new value.
My goal is to print in the SWV ITM Data Console via prinft-commando .
By the way... why does it different if i uncomment the "_write"-function???
Thank you for your help,
Günther
here you found my main function:
int main(void)
{
HAL_Init();
/* USER CODE BEGIN 1 */
int i;
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
GPIOD -> MODER |= (1<<24); // Set pin 12 (orange LED)to be general purpose output in GPIO port mode register
GPIOD -> MODER |= (1<<26); // Set pin 13 (orange LED)to be general purpose output in GPIO port mode register
GPIOD -> MODER |= (1<<28); // Set pin 13 (orange LED)to be general purpose output in GPIO port mode register
// GPIOD -> MODER |= (1<<30); // Set pin 13 (orange LED)to be general purpose output in GPIO port mode register
// void GPIO_config(void);
while(1)
{
for (i = 0; i < 1000000; ++i); // Delay
GPIOD -> ODR |= (1<<13); // Turn GPIOD pin13 (orange LED) ON
printf("Hello World!");
// GPIOD -> ODR |= (1<<14); // Turn GPIOD pin13 (orange LED) ON
// GPIOD -> ODR |= (1<<15); // Turn GPIOD pin13 (orange LED) ON
ITM_SendChar( 65 ); // Send ASCII code 65 = ’A’
for (i = 0; i < 1000000; ++i); // Delay
GPIOD -> ODR &= ~(1<<13); // Turn GPIOD pin13 (orange LED) OFF
// GPIOD -> ODR &= ~(1<<14); // Turn GPIOD pin13 (orange LED) OFF
// GPIOD -> ODR &= ~(1<<15); // Turn GPIOD pin13 (orange LED) OFF
ITM_SendChar( 65 ); // Send ASCII code 65 = ’A’
printf("TEst %i",i);
}
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_CAN1_Init();
MX_I2C1_Init();
MX_SPI2_Init();
MX_UART4_Init();
MX_ADC1_Init();
/* USER CODE BEGIN 2 */
/*
int Get_ADC_Converted_Value(){
ADC_SoftwareStartConv(ADC2);
while(ADC_GetFlagStatus(ADC2, ADC_FLAG_EOC))
{
return ADC_GetConversionValue(ADC2);
}
}
*/
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
// while (1)
// {
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
// }
/* USER CODE END 3 */
}
2020-01-27 11:09 PM
I think i found my mistake ... CPUClock frequency was not correct.
Default CPU Clock is (in my case) 16Mhz and SWOClock 500kHz.
If the SWO-clock wrong SWV ITM Data Console works but show different ASCII-signs.
Now data will show at the SWV ITM Data Console works fine.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.