2023-04-03 1:01 AM
This is a super super weird one.
My device (STM32F401RC) uses the latest HAL libs vs STM32CubeIDE. USB is configured as device-only, CDC.
It works *perfectly* until i also enable one of the I2C peripherals (HAL, config'ed as I2C slave) and send/recv I2C data.
When i do so the OS (happens with Win10/11, Linux and OS-X) occasionally (every 5-20 sec) drops and re-connects the USB connection to my device.
What's stranger again, it'll only happen when connected via a USB hub. When connected directly to the PC it works ok.
I've also tried different hubs, it happens with all of them.
I've also tried connecting my device though a Total Phase USB analyzer. When its connected to the analyzer and the hub, the error no longer occurs (sigh).
Any ideas??
Thanks in advance!
2023-04-03 2:17 AM
Sounds more like hardware issue to me, i.e. I'd investigate power source/drop, crosstalk between I2C and the USB lines, observe using oscilloscope USB lines maybe even unconnected (maybe loaded by a 15k pulldown mimicking the hub) with and without I2C.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.