2014-01-13 3:02 PM
Hi,
I am currently playing around with the STM32F4 Discovery board and saw that the STM32F407VG contains a second USB port. Connector CN5 is the first one, which is connected to PA11 and PA12 and also described in the examples. The second one needs to be connected on PB14 and PB15, but it seems that it isn't use on the board. It seems to be possible to use the second port by connecting PB14/PB15 to D-/D+ (for a USB device), but is it possible to use both USB ports at once? And if so: how can I choose the port in the USB libraries? Does anyone have a simple example or a hint on howt to use it? Thanks in advance, Tim #usb #stm32 #stm32f4 #discovery2014-01-13 3:58 PM
The examples generally target the STM3240G-EVAL board, and will need to be ported for the DISCOVERY board, this may involve removing LCD code and changing pin assignments. You should review the STM3240G-EVAL schematics to better understand connectivity options.
You are referring to the HS port, the examples for the Discovery board normally use the FS port. To switch the code must be compiled with the appropriate defines passed to the compiler. USE_STDPERIPH_DRIVER STM32F4XX USE_STM324xG_EVAL USE_USB_OTG_HS USE_EMBEDDED_PHY vs USE_STDPERIPH_DRIVER STM32F4XX USE_STM324xG_EVAL USE_USB_OTG_FS2014-01-14 8:58 AM
Thanks clive1. The schematics of the board were indeed very helpful and I guess that's exactly what I was looking for.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.