2019-11-20 4:00 AM
Hi,
Actually we require to do bootloader development for self program without any external host like ST-Link or debuggers in STM32F205xx controller, we should program from USB mass storage device.
Our requirement is once we connected pen drive, have to check and read .HEX file if available, after reading it should be update self program according bootloader code. Is this possible to implement for F205 controller..
Kindly help on this regard.
Thank you.
2019-11-20 4:48 AM
Should be a workable example for the STM32F407 DISCO board. FW Upgrade as I recall. Other IAP examples are also available. Yes the F4 USB code should be compatible with the F2.
2019-11-20 5:31 AM
Thanks for your reply. Can you share the source code links for migrating to F2 series.
2019-11-20 6:20 AM
In Keil I think I could just change the target CPU..
https://www.st.com/en/embedded-software/stsw-stm32068.html
STM32F4-Discovery_FW_V1.1.0\Project\FW_upgrade
From the HAL/Cube side of the pond..
STM32Cube_FW_F4_V1.24.0\Projects\STM32F4-Discovery\Applications\FatFs\FatFs_USBDisk
STM32Cube_FW_F4_V1.24.0\Projects\STM324xG_EVAL\Applications\USB_Host\FWupgrade_Standalone
STM32Cube_FW_F2_V1.8.0\Projects\STM322xG_EVAL\Applications\USB_Host\FWupgrade_Standalone
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.