2015-12-15 8:20 AM
I have problem with STM32f103 FatFS library.
If I start it withSD_SetDeviceMode(SD_POLLING_MODE) everything works OK.
But when I change it to
SD_SetDeviceMode(SD_DMA_MODE) it is fired HardFaultHandler.
Thread #1 <
main
> (Suspended : Breakpoint)
HardFault_Handler() at exception_handlers.c:328 0x800011c
<
signal
handler called>() at 0xfffffff1
0x0
<
signal
handler called>() at 0xfffffff9
SD_ReadBlock() at sdcard.c:916 0x800344c
disk_read() at diskio.c:95 0x80003ec
move_window() at ff.c:745 0x80004f6
check_fs() at ff.c:2 184 0x800051a
find_volume() at ff.c:2 258 0x800060a
f_mount() at ff.c:2 441 0x8000984
<...more frames...>
JLinkGDBServerCL.exe
[HardFault]
Stack frame:
R0 = 10002000
R1 = 00000001
R2 = 00002A80
R3 = 10001FFF
R12 = 0000000D
LR = FFFFFFF9
PC = 00000000
PSR = 20000041
FSR/FAR:
CFSR = 00020000
HFSR = 40000000
DFSR = 00000001
AFSR = 00000000
Misc
LR/EXC_RETURN= FFFFFFF1
Problem is fired when Reading FatFS->win. It is 512bytes buffer.
I align it by
BYTE __attribute__ ((aligned)) win [512];
sdio dma reading initialization is:
static void DMA_RxConfiguration(uint32_t *BufferDST, uint32_t BufferSize)
{
DMA_InitTypeDef DMA_InitStructure;
DMA_ClearFlag(DMA2_FLAG_TC4 | DMA2_FLAG_TE4 | DMA2_FLAG_HT4 | DMA2_FLAG_GL4);
/* DMA2 Channel4 disable */
DMA_Cmd(DMA2_Channel4, DISABLE);
/* DMA2 Channel4 Config */
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)SDIO_FIFO_Address;
DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)BufferDST;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;
DMA_InitStructure.DMA_BufferSize = BufferSize / 4;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Word;
DMA_InitStructure.DMA_Mode = DMA_Mode_Normal;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;
DMA_Init(DMA2_Channel4, &DMA_InitStructure);
/* DMA2 Channel4 enable */
DMA_Cmd(DMA2_Channel4, ENABLE);
}
#stm32-fatfs-sdio-dma-hardfault
2015-12-15 8:43 AM
Make sure the stack is sufficiently large, and that if you DMA into the stack (local/auto variables) that the scope is valid over the entire DMA transaction.
I'd guess your DMA is trashing the stack, or other parts of the memory arena. You might want to fill unused memory, or guard regions around the DMA area, and confirm it's not exceeding its bounds.2015-12-15 11:39 PM
Stack is laaaaarge
__Main_Stack_Size = 4096;
Problematic is first DMA read, data buffer is 512B, so it can't trash the stack.
It is ''empty'' project, only hardware initialization and SD card mounting
NVIC_Configuration();
Status = SD_Init();
Status = SD_GetCardInfo(&SDCardInfo);
if (Status == SD_OK) // ----------------- Select Card --------------------------------
Status = SD_SelectDeselect((u32) (SDCardInfo.RCA << 16));
if (Status == SD_OK) // Set Device Transfer Mode to DMA
Status = SD_SetDeviceMode(SD_DMA_MODE); // SD_POLLING_MODE SD_DMA_MODE SD_INTERRUPT_MODE
fr = f_mount(&FatFs, ''0:'', 1);
When main() function started, stack pointer is 0x20009fe8
Before HardFault is stack 0x20009cd8
In HardFault handler stack is 0x20009c98
I think stack is OK
there are registers on HardFault_Handler (before HardFault_Handler_C)
General Registers General Purpose and FPU Register Group
r0 268496896
r1 512
r2 0
r3 1110443404
r4 42
r5 512
r6 536874840
r7 536874840
r8 512
r9 9
r10 3372728174
r11 3342186858
r12 13
sp 0x20009c98
lr 4294967281
pc 0x800011c <
HardFault_Handler
>
xpsr 1627389955
MSP 536911000
PSP 626494284
PRIMASK 0
BASEPRI 0
FAULTMASK 0
CONTROL 0
2015-12-17 2:14 PM
__process_stack_size big enough?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.