2017-06-09 2:23 AM
Hello,
I have a
weird
behavior with STM32F091RCT6 SPI Peripheral on Nucleo Evaluation Board.I want to interface with a 25LC640 SPI eeprom with 8 bits data mode
When i want to send a byte, i see On Oscilloscope 16 clocks pulse instead of 8 !!
I have tested several setting, i have the good number of pulses for 9 bits data size and more .
Context :
STM32F091RCT6
HAL library 1.6
Keil IDE & compiler : 5.06
SPI2 Peripheral on Port B Pin 13,14,15 Master Mode without NSS pin
SPI setup like this :
void MX_SPI2_Init(void)
{hspi2.Instance = SPI2;
hspi2.Init.Mode = SPI_MODE_MASTER; hspi2.Init.Direction = SPI_DIRECTION_2LINES; hspi2.Init.DataSize = SPI_DATASIZE_8BIT; hspi2.Init.CLKPolarity = SPI_POLARITY_HIGH; hspi2.Init.CLKPhase = SPI_PHASE_1EDGE; hspi2.Init.NSS = SPI_NSS_SOFT; hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_4; hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi2.Init.TIMode = SPI_TIMODE_DISABLE; hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi2.Init.CRCPolynomial = 8; hspi2.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE; hspi2.Init.NSSPMode = SPI_NSS_PULSE_DISABLE; if (HAL_SPI_Init(&hspi2) != HAL_OK) { Error_Handler(); }}
__HAL_RCC_SPI2_CLK_ENABLE();
__HAL_SPI_ENABLE(spiHandle); /**SPI2 GPIO Configuration PB13 ------> SPI2_SCK PB14 ------> SPI2_MISO PB15 ------> SPI2_MOSI */ GPIO_InitStruct.Pin = GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.Alternate = GPIO_AF0_SPI2; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);Sending function :
static uint8_t eep_SpiSendByte (uint8_t data)
{while (( EE_SPI->SR & SPI_SR_TXE_Msk) == RESET); // Wait for empty transmit buffer
EE_SPI->DR = data;while (( EE_SPI->SR & SPI_SR_RXNE_Msk) == RESET); // Wait for received buffer with new data
return (uint8_t)EE_SPI->DR;}
Thanks
#stm32f091-spi-spi_datasize_8bit #hal-v1.6Solved! Go to Solution.
2017-06-14 9:08 AM
Edit: why is this being moderated ? Syntax highlighter ?
I strongly suspect they check every code snippet with <LARGE DATABASES> for copyright protection violations before rolling it out.
And there seems to be a list of code words that trigger a detour through moderation.
2017-06-14 10:18 AM
Yes that would make sense...
2017-06-16 1:37 AM
I test the solution given by waclawek.jan and i understood it with Kraal explanation.
Thanks a lot !!
Now i could seed 4 separated bytes on scope. But it work if I put a little delay after the last wrote of the data register to received the the reading byte !
I have tested three solutions , and I think there is a strange behavior of Rx Fifo in STM32F091. Only one with the delay works.
Normal Case Doesn't work all reading value are 0 :
static uint8_t eep_SpiReceiveByte (void)
{ while ((EE_SPI->SR & SPI_SR_TXE_Msk) == RESET); // Attente du buffer de transmission vide *(volatile uint8_t*)&EE_SPI->DR = 0xFF; // 8 cycles d'horloge while ((EE_SPI->SR & SPI_SR_RXNE_Msk) == RESET) return (uint8_t)EE_SPI->DR;}Corrected previously case with delay :
static uint8_t eep_SpiReceiveByte (void)
{ while ((EE_SPI->SR & SPI_SR_TXE_Msk) == RESET); // Attente du buffer de transmission vide *(volatile uint8_t*)&EE_SPI->DR = 0xFF; // 8 cycles d'horloge while ((EE_SPI->SR & SPI_SR_RXNE_Msk) == RESET) delayUS(10); return (uint8_t)EE_SPI->DR; }Tested Reception with Rx Fifo Level in FRLVL[1:0] in Status Register like this :
static uint8_t eep_SpiReceiveByte (void)
{ while ((EE_SPI->SR & SPI_SR_TXE_Msk) == RESET); // Attente du buffer de transmission vide *(volatile uint8_t*)&EE_SPI->DR = 0xFF; // 8 cycles d'horloge while ((EE_SPI->SR & SPI_SR_RXNE_Msk) == RESET) while ((EE_SPI->SR & 0x0600) != 0x0000) while ((EE_SPI->SR & 0x0600) != 0x0200) return (uint8_t)EE_SPI->DR;This last method work for the first eeprom reading byte, after we have always the same value.
Whe also tested empty Transmit buffer before transmit with this method :
static uint8_t eep_SpiReceiveByte (void)
{ while ((EE_SPI->SR & 0x1800) != 0x0000) while ((EE_SPI->SR & SPI_SR_TXE_Msk) == RESET); // Attente du buffer de transmission vide *(volatile uint8_t*)&EE_SPI->DR = 0xFF; // 8 cycles d'horloge while ((EE_SPI->SR & SPI_SR_RXNE_Msk) == RESET) return (uint8_t)EE_SPI->DR;Nothing better !
It appears that RXNE is not a good information to now if a valid byte is in the receveid buffer.
How does the Rx Fifo work ?
2017-06-16 4:47 AM
while ((EE_SPI->SR & SPI_SR_RXNE_Msk) == RESET)
You want to put a semicolon ; or an empty compound statement {} after this statement.
JW
2017-06-16 7:26 AM
It's work now ................
Oupsss
>:(
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.