2023-05-26 6:04 AM
Hello everyone,
I need help because i wanted to use USB VCP for communicating from my STM32 to an arduino via USB-Serial converter.
I thought this MCU was good enough for that. But it seems to have a memory problem.
After creating a new project and enabling the "Virtual Port Com" in "USB_DEVICE Mode and Configuration", I generate the code and compile, and get the following error:
/home/luispl/st/stm32cubeide_1.12.0/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.linux64_1.0.200.202301161003/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld: emwaver_usbtest_f042.elf section `._user_heap_stack' will not fit in region `RAM'
/home/luispl/st/stm32cubeide_1.12.0/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.linux64_1.0.200.202301161003/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld: region `RAM' overflowed by 376 bytes
collect2: error: ld returned 1 exit status
make: *** [makefile:68: emwaver_usbtest_f042.elf] Error 1
Any help would be appreciated. I really want to make this MCU work with virtual com port. I find it weird that this one doesn't work and has 32kb flash, but the bluepill module works fine and has 64kb flash. It's just double. Does the USB driver cost that much memory? How complex can it be..
Solved! Go to Solution.
2023-05-26 7:19 AM
It's fixed. It was the buffer that was too big, I changed from 1024 bytes to 128 and it worked
2023-05-26 7:19 AM
It's fixed. It was the buffer that was too big, I changed from 1024 bytes to 128 and it worked
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.