2015-07-06 8:30 AM
Hello everyone.
At my device I have to make an opputunity to load a firmware through UART interface. I know, that it's possible to do using just USB-UART converter. At the F1 series for this purpose I should set the BOOT0 and BOOT1 pins, but I don't have those at my STM32F0 uC. In that case, I want to ask the community: how can I organise all of the processes of loading firmware through USB at my controller? If it's possible, provide me please some code examples and schematics. I use STM32F0DISCOVERY board for development, in future I will have only the same controller, as installed at the board.I look forward for your answers. #stm32 #usb #uart #usart #stm32f02015-07-06 11:20 AM
Ok, so which part specifically are you using that doesn't have a BOOT[0] pin?
Would suggest you review the documentation for the STM32 System Loader, and USART protocol. Also look at the Flash Loader Demonstrator, with source, and other Open Source equivalents.2015-07-07 12:17 AM
Sorry, I made a mistake.
I mean, I have only BOOT0 pin at the uC.2015-07-07 2:21 AM
Hi n.yuriy,
BOOT1 isn't a pin but a bit that you may update using the option bytes.With the STLink Utility, you can update the value of ''nBoot1''. WHen nBOOT1 is checked and BOOT0=1, you will boot from System Memory.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-07-07 4:41 AM
Dear Mayla, thank you very much for your answer. I'll try to use it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.