2020-06-11 2:18 AM
Hi,
can you please share me the SDK , Peripheral library code,Example code of the STM32F051C8T6TR . As i am new to this controller
2020-06-11 2:39 AM
Find your MCU on the st.com website, click Tools & Software, then Embedded Software.
Start with STSW-STM32048 STM32F0xx standard peripherals library or STM32CubeF0.
A slow and annoying registration/login process might be required to download them.
2020-06-11 4:04 AM
Hi @Chandana ,
Welcome to STM32 Community!
Please note that ST doesn't provide what you call SDK for STM32, but a firmware package with drivers and examples.
It is the STM32CubeF0 that you may download from https://www.st.com/en/embedded-software/stm32cubef0.html (with Github link).
I recommend you also to have a look to the STM32 Wiki, and mainly the "Getting started" section: https://wiki.st.com/stm32mcu/wiki/Getting_started.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-06-16 3:15 AM
Thanks for reply.
Sorry for the late reply.
I have downloaded the firmware package through the link which you have given but i need to write the code for the STM32F051C8T6TR controller so in the package i didn't find this controller in that it has stm32f030, stm2f032, stm2f042, stm2f070, stm2f072, stm2f091, controller are there .Could you please tell me where to download the STM32F051C8T6TR firmware package.
2020-06-16 3:16 AM
Thanks for reply.
Sorry for the late reply.
I have downloaded the firmware package through the link which you have given but i need to write the code for the STM32F051C8T6TR controller so in the package i didn't find this controller in that it has stm32f030, stm2f032, stm2f042, stm2f070, stm2f072, stm2f091, controller are there .Could you please tell me where to download the STM32F051C8T6TR firmware package.
2020-06-16 3:16 AM
Thanks for reply.
Sorry for the late reply.
I have downloaded the firmware package through the link which you have given but i need to write the code for the STM32F051C8T6TR controller so in the package i didn't find this controller in that it has stm32f030, stm2f032, stm2f042, stm2f070, stm2f072, stm2f091, controller are there .Could you please tell me where to download the STM32F051C8T6TR firmware package.
2020-06-16 9:31 AM
You are speaking about the available examples which depend on the boards provided by ST.
But as device, STM32F051 are supported by the same firmware package common for all STM32F0 parts.
You can start by generating your own example for this device using STM32CubeMX.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-06-16 10:41 PM
If it is your first ever STM32 microcontroller project, then I'd suggest getting a STM32F0 based discovery or nucleo board first, for which there are example projects. Review the feature set of the boards, chose one which is the best match for the feature set required for your project.
Now you can start with the examples. Work towards understanding how each peripheral works, replacing each library function call with your own. Write your own peripheral drivers based on the descriptions and examples in the reference manual.
Then you are ready to start working with your MCU, as the peripherals are compatible within the series.
2020-06-16 11:08 PM
You'd select the exact part in your project. The different parts you tried to enumerate just have slightly different combinations of memories and peripherals. All very similar.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.