2025-05-20 2:46 AM
Hi,
I'm currently using STM32CubeMX V6.12.0 to initialise the peripherals on an STM32H753 processor, and I had a couple of questions:
1. How do I enable & then configure the CAN Transciever Delay Compensation within CubeMX?
2. Is there a mechanism for limiting the number of auto-retransmissions in the event of a CAN Error? I currently have that option unchecked but when doing bench-top testing it's clogging up the processor and causing it to run slowly.
Many Thanks,
Crispin
Solved! Go to Solution.
2025-05-23 3:25 AM
Hello @CZuercher_Ilm
First let me thank you for posting.
About the CAN Transciever Delay Compensation, it is not possible to configure it from within STM32CubeMX.
For more details, I will redirect your question to the STM32MCUs forum as it is a better place to get help with the CAN configuration.
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-23 3:25 AM
Hello @CZuercher_Ilm
First let me thank you for posting.
About the CAN Transciever Delay Compensation, it is not possible to configure it from within STM32CubeMX.
For more details, I will redirect your question to the STM32MCUs forum as it is a better place to get help with the CAN configuration.
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-23 6:45 AM
@CZuercher_Ilm wrote:2. Is there a mechanism for limiting the number of auto-retransmissions in the event of a CAN Error? I currently have that option unchecked but when doing bench-top testing it's clogging up the processor and causing it to run slowly.
You can disable completely the retransmission with Init.AutoRetransmission = DISABLE.
2025-05-28 12:06 AM
Hi Saket,
Yes; I have disabled this particular bit of functionality, however in the fullness of time I need to be able to limit the number of retransmission attempts to say, 6, before that message is abandoned.
Is there a way of doing this elegantly and efficiently, without having to call interrupts etc.?
Many Thanks,
Crispin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.