2017-11-03 2:21 PM
Hello.
I want to implement USB-CDC device on STM32F070P6. I've generated the needed code using STM32CubeMX but it doesn't seems to work.
I can't see USBD_CDC_Init to be called, thus when the device is flashed I get this error:
[15798.097292] usb 2-7: device descriptor read/64, error -71
[15798.325291] usb 2-7: device descriptor read/64, error -71[15798.553272] usb 2-7: new full-speed USB device number 96 using xhci_hcd[15798.673212] usb 2-7: device descriptor read/64, error -71[15798.901228] usb 2-7: device descriptor read/64, error -71[15799.129268] usb 2-7: new full-speed USB device number 97 using xhci_hcd[15799.129474] usb 2-7: Device not responding to setup address.[15799.337467] usb 2-7: Device not responding to setup address.[15799.545254] usb 2-7: device not accepting address 97, error -71[15799.665263] usb 2-7: new full-speed USB device number 98 using xhci_hcd[15799.665470] usb 2-7: Device not responding to setup address.[15799.873426] usb 2-7: Device not responding to setup address.[15800.085156] usb 2-7: device not accepting address 98, error -71[15800.085195] usb usb2-port7: unable to enumerate USB deviceAm I missing something?#stm32f070 #usb-cdcWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.