2021-03-16 1:40 PM
Hello,
We have purchased the STM32F769I-DISCO KIT as we plan to use STM32F769I in USB audio IN/OUT application.
I am trying to make "STM32CubeExpansion_USBAudioStreaming_V1.0.0" example provided by ST working. So far:
In our application we will have a codec similar as the one (WM8994) on the STM32F769I-DISCO KIT and we need to stream IN and OUT thru that codec. On the STM32F769I-DISCO KIT there is "Line in" connector to the WM8994 codec. And I am trying to make recordings working using the "Line in". As the example uses the PDM MEMS microphones I have to make some changes.
In the above example I have noticed a macro which seems to switch between the MEMS microphones and the WM8994 "Line in" (INPUT_DEVICE_ANALOG_MIC)
In the file stm32f769i_discovery_audio_ex.c I have modified the lines :
...
static uint16_t AudioIn_Device = INPUT_DEVICE_ANALOG_MIC;
...
return BSP_AUDIO_IN_InitEx(INPUT_DEVICE_ANALOG_MIC, AudioFreq, BitRes, ChnlNbr);
...
I still have in my project preprocessor the variables
...
USE_USB_AUDIO_RECORDING=1
USE_AUDIO_DFSDM_MEMS_MIC=1
Pretty much this is what I see needs to be adjusted but still my recordings from "Line in" does not work. I recorded only silence.
Anyone who knows what may be wrong?
Thank you
Dimitar
2021-04-13 8:13 AM
No your changed code not help . Example record is prepared only for DIGITAL MIC.
You need write your own code for record line in.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.