2017-02-27 1:41 AM
Greetings to all the GEEKS.
Well i am looking for STM32 microcontroller that has usb host capability as well as it can interface with micro sd card or sd card. The reason for usb host capability is --- I want to store the data on to usb pen drive that is fat or fat32 formatted. I want the interface with micro sd card or sd card for the same reason. If usb pen drive is not attached then i want to store data on to micro sd card or sd card.
Any advice will be helpful. I don't mind the usb host speed i.e. i am okay if i don't get usb host capability on full speed.
#usb-host #micro-sd-card #sd-card2017-02-27 2:19 AM
The USB OTG can work as host. It is present on STM32F105/F107/F2xx/F4xx/F7xx/L4x5/L4x6 series.
All of them have a an SPI than can be used for the SDCARD (in SPI mode)
You will get better performances by using
STM32F2xx/F4xx/F7xx because they embed a SDIO peripheral ideal for the SDCARD.
regards,
Max
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.