2013-03-01 3:08 AM
I'm using drivers from VCP_V1.3.1_Setup.exe. It works fine on win7 x32, but on w8 x64 installator says something like ''it was supposed to run me under x32'', so my device does not work there.
Where I can download such drivers? #stm32-usb-x642013-03-01 7:01 AM
Wouldn't you use VCP_V1.3.1_Setup_x64.exe ??
If the driver isn't signed, I don't recall if it is, you'd have to turn that feature off in Win 8. In under a week I've had a Windows 8 system totally destroy itself in normal operation, something I haven't seen in well over a decade for other releases. So I'm completely impressed with it so far.2013-03-05 3:43 AM
thanks for help, I did not realise to search the same driver name +x64 on the end.
it works on w8, but I dont have time to do proper tests now. We are going to use a tablet computer there, now we are considering acer iconia tab with w7, but, anyway, sooner or later, we will have to switch to w8.2013-03-05 3:53 AM
I could swear it is in the same package as the other driver, and evident when the download is unpacked.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.