2025-07-19 7:20 AM - last edited on 2025-10-21 4:09 AM by Amel NASRI
I have tried USB examples for Stm32F070, F401, F407 Black board and calling a single "CDC_Transmit_FS" function to print a string but none is working. The hcdc->TxState value is some garbage big value so it always stay busy and also not getting interrupts for USB receive as I have put break points in it too. The STM32 device show up as "composite" instead of VCP.
For configuration it is RCC->Bypass Clk, USB connectivity->Device Only, USB_Device->VCP, heap size->0x1000.
2025-10-23 6:52 AM
Hi @Lakshay
Would you point me directly to example firmware not working, and full hardware setup including board revision?
If your device enumerates incorrectly or driver installation is stuck, changing the PID is a workaround to force the OS to reload the USB driver and re-enumerate the device properly.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.