2015-10-12 8:27 AM
Hi All,
i have a problem with the managment of the UART Error.Particularly when the error occurs in ''HAL_UART_ERROR_ORE'', the device is locked and I can not clear the error.I tried using the following instructions, under callback error funcion:void HAL_UART_ErrorCallback(UART_HandleTypeDef *huart){__HAL_UART_SEND_REQ (Huart, UART_RXDATA_FLUSH_REQUEST);uint8_t tmp = (uint8_t) huart-> Instance-> RDR;__HAL_UART_CLEAR_OREFLAG (Huart);huart->ErrorCode = HAL_UART_ERROR_NONE;}But the error flag continues to recover, and the UART remains locked.Thank you,Mauro. #stm32 #uart #hal2015-10-12 10:57 AM
Does the error reoccur even if you stop the incoming data source?
JW2015-10-12 2:40 PM
An error callback usually means something is wrong with the transmission. Rather than work it in the callback; perhaps step through the transmission and receive routines and see which line is triggering the error. I havent looked this up but, I want to say the ORE is an buffer overrun event. The error might be getting cleared in the callback but being set again by the buffer still running over its banks.
2015-10-13 12:00 AM
Hi waclawek,
Yes, the error persists even when the data on the UART are stops.The error is generated by me, by sending a string of 3 characters and stopping the debug code in the reception of the first character.2015-10-13 10:28 AM
> The error is generated by me, by sending a string of 3 characters and stopping the debug code in the reception of the first character.
Ah, so you wanted to test what happens? Do you display the UART registers in the debugger during this? Debugger can be intrusive; OTOH I don't understand the mechanism why this would cause stuckup. As NStuff wrote above, the HAL ''driver'' appears to clear the error itself directly in the ISR before calling the callback. Observe the UART registers in the debugger - does the real overflow flag get cleared or not? Jan2015-10-19 11:28 PM
Hello,
yes, I was testing the behavior of the serial on error.From debugger I also checked the registers of the UART, and I noticed that the bit error is not cleared, and the perifrica stuck.Thank you,Mauro.2015-10-27 6:51 AM
Hello,
which STM32 series are you using? I think HAL driver implementations differ a little bit from one family to the otherWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.