2025-03-07 7:18 AM
Hi, my current issue is that after implement Self test library for a stm32h5 the basic things like STL_SCH_Init() works fine but when i try to run the flash test the STL_SCH_ConfigureFlash fails, the status says STL_ERROR.
How i run the test:
I also use the CRC tool that is required for the test with the full flash range.
So my question is why the configureFlash fails?, because even if i define small ranges for the test it still fails the configuration and i check and re-check the ranges.
Thanks for reading.
2025-03-13 8:13 AM
Thanks for your reply, it was a flash offset that misaligned the flash memory.
2025-03-13 8:54 AM
Sorry I delete by mistake my original reply. Yes, the tested area has to be set carefully. It has to start at 1KB boundary and end at binary end aligned at word boundary. Binary has to be continuous without any gaps in between code sections. Valid CRC value must be stored for each tested 1KB tested memory section at CRC-area else test execution fails. Note ST Cube Programmer computes CRCs for memory sections occupied by code exclusively. For more details pls study the STL user guide.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.