2025-10-29 5:16 AM
Hi,
I just stumbled upon something interesting (at least for me). For my current project I need to store data from a float array with two elements in an uint8_t array with eight elements. I use the following code to archive this:
pnt = (uint8_t*)out;
for(i = 0; i < 8; i++)
{
uart_tx_buffer[i + 3] = *(pnt + i);
}While it technically works, the bytes from each float element get stored in the buffer in a reversed order. I can give you an example from what I am looking at in the debug session. The float array has the values out = {0x41bef708, 0x4478a1d7}. So the result I exacted for the buffer is uart_tx_buffer = {xx, xx, xx, 0x41, 0xbe, 0xf7, 0x08, 0x44, 0x78, 0xa1, 0xd7}. But in reality it looks like this uart_tx_buffer = {xx, xx, xx, 0x08, 0xf7, 0xbe, 0x41, 0xd7, 0xa1, 0x78, 0x44}.
At first I thought the values in the buffer are completely random because I made a mistake. It took me a while to figure this out. What is the reason why this happens? Can I avoid this, because now I would have to shift all these bytes around.
I am using STM32CubeIDE 1.19.0 to program a NUCLEO-F429ZI.
2025-10-29 5:45 AM
This issue is called endianness, and refers to an architecture's way of storing and accessing objects greater than 1 byte (usually the minimal size for an object in memory).
https://en.wikipedia.org/wiki/Endianness
If it comes to communication between different systems, either use ASCII/text format, or stick to one endianness.
As an example, CANopen defines "Little Endian" for all message transfers.
2025-10-29 5:52 AM
If you want the same memory order, use memcpy.
uint8_t one[8];
float two[2];
memcpy(two, one, 8);If byte order needs swapped, you can use __REV to reverse endianness:
uint8_t one[8];
float two[2];
two[0] = __REV(((uint32_t*)one)[0]);
two[1] = __REV(((uint32_t*)one)[1]);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.