2025-09-29 6:33 PM
Hello,
I have a project using the spirit MP3 Decoder. I am in the process of moving this project over to a FreeRTOS based project using the STM32F411. FreeRTOS only supports hardware floating point for this chip and the spirit MP3 decoder is provided as a library only supporting software floating point.
What is required for me to get a new build of the Spirit MP3 deocder re-compiled supporting hardware floating point?
Can ST provide this re-compiled library?
Thanks
Stuart
2025-09-30 4:00 AM
Almost the same question was asked here.
2025-09-30 5:05 PM
Yeah, i saw the post, but in the response it says that the company doesn't exist anymore....
But they do have a website.
Can you confirm that this is the same company? (their logo is the same)
Thanks
2025-11-28 7:34 AM
@SORei.1 wrote:
Can you confirm that this is the same company? (their logo is the same)
Most probably yes. To my knowledge the company name is DSP spirit.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.