2024-11-18 10:11 AM
I am using the Nucleo-H743ZI, with a SPI ISR I wrote originally on the STM32H7B3I-DK board. However, when I use
volatile uint8_t rxBuffer;
volatile uint8_t txBuffer;
*((__IO uint8_t *)&hspi->Instance->TXDR) = txBuffer;
//or
rxBuffer = *((__IO uint8_t *)&hspi->Instance->RXDR);
I get a syntax error on the Nulceo. I checked the stm32h7xx_hal.c file and they use these two lines for the default SPI handler. I have stm32h7xx_hal.h included, but still have a syntax error... wondering if anyone knows what may be going wrong.
I'm not sure why there is no error on my STM32H7B3I-DK board, but there is on the Nucleo.
Solved! Go to Solution.
2024-11-18 10:57 AM
I am using CubeIDE, the thing is that it doesn't show up in the Problems or console log. It just underlines yellow and has the yellow question mark... i found somewhere else in my code that required me to add "-u _scanf_float" to my G++ linker and now there is no longer an errror...
2024-11-18 10:28 AM
@EthanMankins wrote:I get a syntax error on the Nulceo
You mean you get a syntax error from the compiler, surely?
Post the actual error.
You haven't said what IDE/compiler you're using, but if it's STM32CubeIDE, copy & paste the text (not a screenshot) from the 'Console' window.
2024-11-18 10:57 AM
I am using CubeIDE, the thing is that it doesn't show up in the Problems or console log. It just underlines yellow and has the yellow question mark... i found somewhere else in my code that required me to add "-u _scanf_float" to my G++ linker and now there is no longer an errror...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.