2015-12-02 9:22 AM
Hi,
I'm
using the
STM32F407
with
USB
Host
library
, in high-speed.I want to
communicate via
USB
with
a smartphone
.When
i send
a
packet of
64 bytes
everything works
.If I send a
packet
, for example,of
94
bytes
,the first time
send
all
94
bytes
,the second time I
tried again
to
send
94
bytes
or
less
,the
smartphone
receives
the last
94
- 64
=
30
bytes
.Why?
Thisis my code
for
sending
: uint8_t do_ping = 1; uint8_t buff[512]; sprintf(buff,''CAN source address: %d \n TSC1 speed [rpm]: %d '' ''\n Override Control mode: \n Override priority: \n'', buff_TSC1.address, speed_rpm); USBH_Delay(800); while(USBH_OK != USBH_BulkSendData (&hUSB_Host, buff, strlen(buff), pipe_numOUT, do_ping)); USBH_Delay(500);Someone can
explain me how
sending
multi
packet
? Thank you #usbh #stm32 #usb #multi-packet2018-04-25 11:28 PM
Hi, do you have any clue on this issue? I also have similar question about whether the STM32Cube USB Host library support the multi-packets transfer too.
To simplify the question, I test the sample application 'USB_Host/MSC_Standalone' of
STM32Cube V1.17 on STM32F41G EV board. In this sample, I configure the USB to high speed mode, and I change the data which will be written to the USB pen drive from a short string to a 1024 bytes one, which is 2 times of the End Point size (max packet size) of the USB pen drive. it will make
USBH_BulkSendData() specify 1024 in length parameter and further make PKTCNT field defined within OTG_HS_HCTSIZx register to be 2 packet.
After the USBH_BulkSendData() return with URB_DONE, I can't receive the CSW which should acknowledge from the USB pen drive when I invoke USBH_BulkReceiveData(). And the debug on USB pen drive show it actually receive the CBW specify a 1024 bytes length data will be sent then receive nothing later. In the case of writing data to this USB pen drive with PC instead of STM32F41G board, this pen drive is capable to receive USB transfer with mluti-packets up to 64K bytes.
By the way, description of multi packet transfer feature could be found with official user manual 'UM1734, STM32Cube USB device library', but I can't find the same feature on host side manual 'UM1720, STM32Cube USB host library'
Best Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.