2019-04-02 11:21 PM
I have this attribute in my code:
#define PHY_ETHTORAM_ATTRIBUTE __attribute__ ((section(".sram2"), aligned(4)))And for example, in my code:
// Ethernet Rx MA Descriptor
volatile __attribute__((aligned(32))) PHY_ETHTORAM_ATTRIBUTE ETH_DMADescTypeDef DMARxDscrTab[RXBUF];
..........And I have this problem:
Output/test.elf section `.bss' will not fit in region `SRAM1'And I know, that this problem is in linker script...
And my memory is here:
/*
* STM32F427ZIT6 memory map - GNU ld linker script file
*/
MEMORY
{
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 2048K
CCMRAM (rw) : ORIGIN = 0x10000000, LENGTH = 64K
SRAM1 (rw) : ORIGIN = 0x20000000, LENGTH = 112K
SRAM2 (rw) : ORIGIN = 0x2001C000, LENGTH = 16K
BKPSRAM (rw) : ORIGIN = 0x40024000, LENGTH = 4K
}
INCLUDE Linker/Sections.ldAnd Sections.ld is in attachment.
Complete error messages are here:
Any idea, how to change linker script to function code? And what actually happened?
2019-04-03 12:05 AM
The error's saying
Check the linker map file. It'll have a .map extension. If you can't find it, it may have to be turned on.
Perhaps you've accidentally overdimensioned or put something in the wrong section. You'll find that by reading the map file carefully.
If there are no errors in the code, the map file will show if and where there's some space. If you find space, you might determine what you can move there using the same method you used to put DMARxDscrTab[RXBUF] into SRAM2.
2019-04-03 12:19 AM
2019-04-03 2:31 AM
You're looking for the part starting with
.bss 0x200000c0 0x21ba0
0x200000c0 __bss_start__ = .
0x200000c0 _sbss = .
and ending with
*(.bss_end .bss_end.*)
0x20021c60 . = ALIGN (0x4)
0x20021c60 __bss_end__ = .
0x20021c60 _ebss = .
you want also look at noinit and the ._check_stack after that - the result should not "overhang" into sram2.
The biggest consumption there is heap_sram1 0x8000 and buffers? in ./LIBRARY/ETH-STM32-LwIP/MODULE/src/core/memp.o
0x13253 . Those two alone fill almost completely sram1.
JW
2019-04-03 2:42 AM
I have heap_sram1 declare here:
/* heap for FreeRTOS */
static __attribute__ ((aligned (64))) uint8_t heap_sram1[32 * 1024];
const HeapRegion_t xHeapRegions[] = {
{ heap_sram1, sizeof(heap_sram1) },
{ NULL, 0 }
};
/* and in main */
vPortDefineHeapRegions( xHeapRegions );And other size is for LWIP:
#define MEM_SIZE (16*1024)I tried to modificate it, and program is now build OK. But program crashed here:
vApplicationMallocFailedHookAnd my modification is:
/* memory modification */
#define MEM_SIZE (2*1024)
static __attribute__ ((aligned (64))) uint8_t heap_sram1[8 * 1024];
const HeapRegion_t xHeapRegions[] = {
{ heap_sram1, sizeof(heap_sram1) },
{ NULL, 0 }
};
2019-04-03 5:30 PM
Like LW's saying. These are the addresses and sizes of the large ones.
.bss.heap_sram1
0x200008c0 0x8000 ./Main/main.o
COMMON 0x200088cc 0x1478 ./HW/serial/serial_port.o
COMMON 0x2000a5a4 0x4013 ./LIBRARY/ETH-STM32-LwIP/MODULE/src/core/mem.o
COMMON 0x2000e5b8 0x13253 ./LIBRARY/ETH-STM32-LwIP/MODULE/src/core/memp.o
Many of lwIP's buffers can be tuned in STM32CubeMX.
2019-04-04 12:13 AM
Yes, it is true. I modificated lwipopts.h and now MCU is working with ETH. :grinning_face:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.