2017-10-30 6:53 AM
Hi,
I've finished building same code for a stm32l053R8 low power project using both IDE's Keil Microvision 5 & Atollic truestudio v5.5.2. Keil MicroVision project build works fine in all of our boards which we designed for the project. But Atollic build not working in some of our boards.
By switching the power, controllers flashed with keil microvision project .bin are starting from the main easily at the first attempt itself.
But, Atollic build .bin file is not getting into the main at the first attempt( requires NRST from debugger manually to reset properly & start from the main code). I've tried debugging using Atollic IDE, but it works fine, the code jumps to the main. Without debugger connected the codedoesn'trun.
What may be the reason for this kind of behaviour in controllers.?
Thanks in advance
#boot #stm32l053 Note: this post was migrated and contained many threaded conversations, some content may be missing.2017-10-31 7:26 AM
I don't know how Cube plays into the differences between the Keil uVision built executable and the Atollic one.
But since you have a working project with a superior tool (also my opinion), why messing with Atollic ?
Isn't this wasted time & effort ?
2017-10-31 7:57 AM
>> I'm not using any iteration bounded clock startup code.
The Cube code has some of these, you should also look at what SystemInit() is doing.
>>
Linker Script (.ld) looks fine too from what i've seen, attached it for your consideration.
/* Highest address of the user mode stack */
_estack = 0x20002000; /* end of RAM */That looks fine.
2017-10-31 8:02 AM
You shouldn't need to use printf(), the point of checkpoints is you can output single characters to confirm flow and arrival at certain points, and then focus on where it gets stuck, or what exactly is happening internally. ie A-Z
It might take a few dozen lines of assembler to set up the USART, and provide output functions, clocking from the HSI/MSI that is already running.
2017-10-31 11:58 PM
My keil uVision5 license going to expire soon, so thought to port the source codes tosome other open sources.Crossworks is it licensed?
2017-11-01 12:02 AM
Hi Clive,
It is very bizarre, by reducing the clock source. I can get the code running at every attempt of power reset. Anyways i got the desired result, but i would love to debug in my leisure time.
Strange behaviour what may be the possible reason.
2017-11-01 10:38 AM
>>Crossworks is it licensed?
As you expect to get paid, people who provide you with tools and services also expected to get paid, and to pay their employees.
Free stuff should come with the expectation of zero support, where either you need to be self sustaining, or you pay going rates for support.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.