2025-05-22 1:32 AM - last edited on 2025-05-22 6:46 AM by Andrew Neil
Hi!
I'm working on a project with an STM32 microcontroller and need to set up a way to update the firmware remotely. The device will be installed in remote locations so I won’t have physical access once it's deployed.
What’s the best way to approach this on STM32?
Any tips or examples would be really helpful.
Thanks!
2025-05-22 1:46 AM - edited 2025-05-22 4:00 AM
You'll need two things:
"OTA" and "Bootloader" would be good search terms; eg,
https://community.st.com/t5/stm32-mcus-products/how-can-i-use-an-esp32-to-update-the-firmware-of-an-stm32-from/m-p/696326/highlight/true#M254867 and the next post in that thread.
PS:
"In-Application Programming" or "IAP" would also be good search terms...
2025-05-22 3:17 AM - edited 2025-05-22 3:17 AM
Hello @Lenor and welcome to the community,
An example is provided at this link using ESP8266 WiFi module to perform an IAP: In Application Programming working on STM32F7. See this link.
2025-05-22 3:50 AM
I was just reading about this, and from what I understand, a common way to do remote firmware updates on STM32 is by using a bootloader that handles receiving and installing the new firmware. The bootloader is stored in the MCU’s flash memory and allows updates without needing external apps. It safely writes the new firmware to the main program area.
There are also third-party software solutions that can help manage updates remotely and make the process easier. For more details, you can check it out here: https://www.flexihub.com/over-the-air-software-update/
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.