2016-11-02 2:52 AM
I am a beginner, I have the Uart dma example code. How can i change the program to receive the continuous data obtained from the TX in RX in a simple way. Here is my main fucntion
&sharpinclude ''main.h''&sharpinclude ''stm32f4xx_hal.h''&sharpinclude ''dma.h''&sharpinclude ''usart.h''&sharpinclude ''gpio.h''/* USER CODE BEGIN Includes */&sharpdefine TXSTARTMESSAGESIZE (COUNTOF(aTxStartMessage) - 1)&sharpdefine TXENDMESSAGESIZE (COUNTOF(aTxEndMessage) - 1)/* Size of Reception buffer */&sharpdefine RXBUFFERSIZE 10/* Exported macro ------------------------------------------------------------*/&sharpdefine COUNTOF(__BUFFER__) (sizeof(__BUFFER__) / sizeof(*(__BUFFER__)))/* USER CODE END Includes *//* Private variables ---------------------------------------------------------*//* USER CODE BEGIN PV *//* Private variables ---------------------------------------------------------*//* USER CODE END PV *//** @addtogroup UART_Hyperterminal_DMA * @{ */ /* Private typedef -----------------------------------------------------------*//* Private define ------------------------------------------------------------*//* Private macro -------------------------------------------------------------*//* Private variables ---------------------------------------------------------*//* UART handler declaration *//* Buffer used for transmission */uint8_t aTxStartMessage[] = ''\n\r ****UART-Hyperterminal communication based on DMA ****\n\r Enter 10 characters using keyboard :\n\r'';uint8_t aTxEndMessage[] = ''\n\r Example Finished\n\r'';/* Buffer used for reception */uint8_t aRxBuffer[RXBUFFERSIZE];/* Private function prototypes -----------------------------------------------*/void SystemClock_Config(void);void Error_Handler(void);/* USER CODE BEGIN PFP *//* Private function prototypes -----------------------------------------------*//* USER CODE END PFP *//* USER CODE BEGIN 0 *//* USER CODE END 0 */int main(void){ /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration----------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* Configure the system clock */ SystemClock_Config(); /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_DMA_Init(); MX_UART8_Init();HAL_UART_MspInit(&huart8); /* USER CODE BEGIN 2 */ /*♯♯-2- Start the transmission process ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ /* User start transmission data through ''TxBuffer'' buffer */ if(HAL_UART_Transmit_DMA(&huart8, (uint8_t*)aTxStartMessage, TXSTARTMESSAGESIZE)!= HAL_OK) { /* Transfer error in transmission process */ Error_Handler(); } /*♯♯-3- Put UART peripheral in reception process ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ /* Any data received will be stored in ''RxBuffer'' buffer : the number max of data received is 10 */ if(HAL_UART_Receive_DMA(&huart8, (uint8_t *)aRxBuffer, RXBUFFERSIZE) != HAL_OK) { /* Transfer error in reception process */ Error_Handler(); } /*♯♯-4- Wait for the end of the transfer ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ /* Before starting a new communication transfer, you need to check the current state of the peripheral; if it�s busy you need to wait for the end of current transfer before starting a new one. For simplicity reasons, this example is just waiting till the end of the transfer, but application may perform other tasks while transfer operation is ongoing. */ while (HAL_UART_GetState(&huart8) != HAL_UART_STATE_READY) { } /*♯♯-5- Send the received Buffer ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ if(HAL_UART_Transmit_DMA(&huart8, (uint8_t*)aRxBuffer, RXBUFFERSIZE)!= HAL_OK) { /* Transfer error in transmission process */ Error_Handler(); } /*♯♯-6- Wait for the end of the transfer ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ while (HAL_UART_GetState(&huart8) != HAL_UART_STATE_READY) { } /*♯♯-7- Send the End Message ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ if(HAL_UART_Transmit_DMA(&huart8, (uint8_t*)aTxEndMessage, TXENDMESSAGESIZE)!= HAL_OK) { /* Turn LED3 on: Transfer error in transmission process */ // BSP_LED_On(LED3); while(1) { } } /*♯♯-8- Wait for the end of the transfer ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ while (HAL_UART_GetState(&huart8) != HAL_UART_STATE_READY) { } /* Infinite loop */ while (1) { }} /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ This is configured for the MCU by taking UART8. Help me its urgent #no-hablo-hal2016-11-15 2:44 AM
Hi sunny.dixon_p,
What are you trying to do exactly?What is going wrong with the code you provided?-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-11-15 5:58 AM
Why are yo polling, and not using interrupts ?
They are designed as immediate responses to external events. > Help me its urgent Do you honestly expect someone else to take the heat for you ????2016-11-15 7:02 AM
What is going wrong with the code you provided?
The OP expressed the desire for it to support reception of data also.http://www.catb.org/~esr/faqs/smart-questions.html#urgent
2016-11-15 8:04 AM
My USART DMA driver does the following:
For TX: - Maintains a queue of pending DMA transfers (of variable length). - I cache the actual data in a TX ring buffer (a little care is need when this wraps - split into - two transfers). - On TC interrupt fetch the next transfer off the queue, set MOAR and NDTR, and re-enable the stream. For RX: - I use a circular buffer for the DMA. - Don't interrupt (I might wait forever for enough data to cause the interrupt). - Poll frequently (SysTick at 1kHz) and test NDTR to see if any new data has been received. - Copy new data into an RX ring buffer (watch the wrapping). - Emit an event to my scheduler to indicate to whoever cares that there is new data to be consumed. No doubt there are better solutions. But it seems pretty robust. I use a scheduler to decouple subsystems, but a synchronous callback would do just as well as an asynchronous event.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.