2024-11-26 7:29 AM
Good morning everyone!
I have a question regarding a USB to UART IC. I’ve seen that the FT231XQ is used in ESP32s to program and communicate via UART. Is it possible to do the same with STM32s?
2024-11-26 7:50 AM - edited 2024-11-26 7:51 AM
Yes.
In this case, all the STM32 sees is a UART connection - it neither knows nor cares whether that came via USB, or from a Real RS232 port, or from anything else.
So, as far as the STM32 is concerned, the FT231XQ (or whatever) is irrelevant - it's all just UART comms.
The built-in UART Bootloader is described in Application Note AN3155, USART protocol used in the STM32 bootloader:
You can also write your own custom bootloader - see, for example Application Note AN4657 STM32 in-application programming (IAP) using the USART:
2024-11-26 10:46 AM
Okay, for Uart it will be possible, but to upload programs to the MCU, will it be possible?
2024-11-27 12:53 AM
@Zero-96 wrote:Okay, for Uart it will be possible, but to upload programs to the MCU, will it be possible?
I don't understand - I just answered exactly that question!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.