2019-11-06 5:12 AM
I want to program my STM32G431-Board with the DFU bootloader.
I’ve already set the configuration to get into the boot-mode with the boot0-Pin. And I explicit configure the read out protection (RDPto level 0.
Also I can connect the device with the USB already in the CubeProgrammer.
My problem is, when I would start programming my code to the target with the CubeProgrammer, there are the following error-message:
Error: RDP level is set to 1 (0xBB), try using Read UnProtect (-rdu) command in order to remove the Read Out Protection.
When I look to the configuration after the error-message, the RDP is on level 0, like I configure before.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.