2025-09-14 5:57 AM - edited 2025-09-14 6:06 AM
In this example, if instead of using HSI I enable HSE, I can’t get memory-mapped mode working on XSPI2.
Baord I am using is NUCLEO-N657X0-Q-C01
I replaced this function
https://github.com/stm32-hotspot/STM32N6_FSBL_Modes/blob/main/LoadAndRun/FSBL/Core/Src/main.c#L119-L198
with my SystemClock_Config
SystemClock_Config(void) {
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the System Power Supply
*/
if (HAL_PWREx_ConfigSupply(PWR_EXTERNAL_SOURCE_SUPPLY) != HAL_OK) {
Error_Handler();
}
/* Enable HSI */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL1.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.PLL2.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.PLL3.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.PLL4.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) {
Error_Handler();
}
/* Wait HSE stabilization time before its selection as PLL source. */
HAL_Delay(HSE_STARTUP_TIMEOUT);
/** Get current CPU/System buses clocks configuration and if necessary switch
to intermediate HSI clock to ensure target clock can be set
*/
HAL_RCC_GetClockConfig(&RCC_ClkInitStruct);
if ((RCC_ClkInitStruct.CPUCLKSource == RCC_CPUCLKSOURCE_IC1) ||
(RCC_ClkInitStruct.SYSCLKSource == RCC_SYSCLKSOURCE_IC2_IC6_IC11)) {
RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_CPUCLK | RCC_CLOCKTYPE_SYSCLK);
RCC_ClkInitStruct.CPUCLKSource = RCC_CPUCLKSOURCE_HSI;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct) != HAL_OK) {
/* Initialization Error */
Error_Handler();
}
}
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL1.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL1.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL1.PLLM = 1;
RCC_OscInitStruct.PLL1.PLLN = 50;
RCC_OscInitStruct.PLL1.PLLFractional = 0;
RCC_OscInitStruct.PLL1.PLLP1 = 1;
RCC_OscInitStruct.PLL1.PLLP2 = 1;
RCC_OscInitStruct.PLL2.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.PLL3.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.PLL4.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) {
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_CPUCLK | RCC_CLOCKTYPE_HCLK
| RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_PCLK1
| RCC_CLOCKTYPE_PCLK2 | RCC_CLOCKTYPE_PCLK5
| RCC_CLOCKTYPE_PCLK4;
RCC_ClkInitStruct.CPUCLKSource = RCC_CPUCLKSOURCE_IC1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_IC2_IC6_IC11;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV1;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV1;
RCC_ClkInitStruct.APB5CLKDivider = RCC_APB5_DIV1;
RCC_ClkInitStruct.IC1Selection.ClockSelection = RCC_ICCLKSOURCE_PLL1;
RCC_ClkInitStruct.IC1Selection.ClockDivider = 3;
RCC_ClkInitStruct.IC2Selection.ClockSelection = RCC_ICCLKSOURCE_PLL1;
RCC_ClkInitStruct.IC2Selection.ClockDivider = 6;
RCC_ClkInitStruct.IC6Selection.ClockSelection = RCC_ICCLKSOURCE_PLL1;
RCC_ClkInitStruct.IC6Selection.ClockDivider = 4;
RCC_ClkInitStruct.IC11Selection.ClockSelection = RCC_ICCLKSOURCE_PLL1;
RCC_ClkInitStruct.IC11Selection.ClockDivider = 3;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct) != HAL_OK) {
Error_Handler();
}And this line
https://github.com/stm32-hotspot/STM32N6_FSBL_Modes/blob/main/LoadAndRun/FSBL/Core/Src/stm32n6xx_hal_msp.c#L102
is changed to:
PeriphClkInitStruct.ICSelection[RCC_IC3].ClockDivider = 48;
In comparison original clock is setup like this:
To new one:
As it can be seen both IC3 clocks are 50 MHz.
With original setup I see this on 0x7000000 address:
With HSE enabled I got this:
What could be wrong?
Solved! Go to Solution.
2025-09-16 9:45 AM - edited 2025-09-17 11:16 PM
I eventually solved it by replacing the drivers and middleware of the project with the latest version.
Link to code: https://github.com/IMProject/IMBootloader/pull/39
2025-09-14 6:18 AM - edited 2025-09-14 6:20 AM
i dont think, changing to HSE as clock source doing something "strange".
But to compare, all clocks+PLL setting have to be same, so adjust it and then try again.
sys not same, maybe others also:
vs
+
Just set the clock tree in Cube , with HSE as source; then try.
2025-09-14 6:32 AM
I used CubeMX just to show that the clock for IC3 is the same in both cases. I don’t use it to generate the code, as you can see from the code I pasted.
2025-09-14 6:43 AM - edited 2025-09-14 6:44 AM
In addition, this is the code where I am trying to enable memory-mapped mode for the MX25UM51245G on XSPI2. It has HSE enabled and working.
https://github.com/IMProject/IMBootloader/blob/master/Bootloader/Adapters/Src/system_clock_adapter.c#L191-L275
Since I was unable to do it, I tested this example that has working HSI + XSPI2. Then I tried to enable HSE + XSPI2, without success.
https://github.com/stm32-hotspot/STM32N6_FSBL_Modes/blob/main/LoadAndRun/FSBL/Core/Src/main.c#L119-L198
2025-09-14 7:25 AM
So use Cube to make the setting with HSE , check : working ?
If ok, just look what/how its doing settings, and you know it. Then use it as you prefer.
2025-09-16 9:45 AM - edited 2025-09-17 11:16 PM
I eventually solved it by replacing the drivers and middleware of the project with the latest version.
Link to code: https://github.com/IMProject/IMBootloader/pull/39
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.