2012-02-22 12:48 AM
Hi all,
I have a problem with SDIO+USB Mass storage device. My eMMC driver now works (in stand alone without USB), and the USB mass storage device also works only if I remove the callbacks functions of init emmc, read and write. That mean my computer detect a new dongle was inserted but without any more info or possibilities to do something. My problem occurs when I want to ''connect'' my callback functions to the eMMC driver the init fails. I think there is an interrupt problem. USB works with high level interrupt and eMMC also. So when USB want to init/read/write the eMMC it is from an interrupt handler. If I play with the interrupt priorities, USB doesn't works at all ... Someone knows this issues ? Thanks. Mikael #usb-msc-+-sdioWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.