2025-02-19 6:17 AM - last edited on 2025-02-20 1:00 AM by FBL
Hi Roger and ST Team,
I am facing the same issue as described by @VH. I am working with the NUCLEO-G0B1RE and TCPP01-M12. and I am trying to use the X-CUBE-TCPP software expansion to this board. My Goal :I need to supply a device with 9V if the power adapter supports it, otherwise fallback to 5V. I originally followed the setup exactly as shown in "How to Create a STM32G0 USB-PD Device with STM32CubeIDE" Youtube video:.However, I encountered an issue where STM32CubeMonitor does not detect any connected device.
Could you please provide guidance on the necessary modifications required to make TCPP01-M12 or the X-CUBE-TCPP work on the NUCLEO-G0B1RE? Are there any key differences between the G071RB and G0B1RE that require specific attention (e.g., clock configurations, UCPD settings, power management, middleware dependencies)?
I appreciate your support!
edit - moved to a new thread from How to port X-CUBE-TCPP to STM32G0B1RE
2025-02-19 8:29 AM
I suggest you these articles and video as a starting point:
Introduction to USB Power Delivery with STM32 - stm32mcu
STM32StepByStep:Getting started with USB-Power Delivery Sink - stm32mcu
How to build an USBPD Sink application using the X-Cube-TCPP software pack - YouTube
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.