2022-05-26 7:08 AM
Hi,
I'm evaluating the WIFI/BLE module 1LV by Murata with a STM32H747-Dicovery board and Murata adapter as reported in the PDF file in https://github.com/Infineon/stm32-connectivity/tree/master/Documentation
The connection works fine (wifi scan OK and connection OK) and now I'm trying to increase the communication performance; the first test, using LWIP stack as server on MCU and ipref client on windows/linux side gave me only 0.15-0.20MB/s (150kBps) that seems to me very VERY slow using SDIO interface (with 25MHz clock).
Do anybody have any clues to increase this bitrate?
What can I change from the test project (https://github.com/Infineon/stm32-connectivity/tree/master/Projects/STM32H747I-DISCO/Applications/wifi_scan) to increase WIFI performance?
Do you also think that LWIP stack is the correct "library" to have good performance (at least 2.5-3.0MB/s)
Thanks
2022-05-26 8:02 AM
I believe 1MB/s is achievable with LwIP stack, if SDIO interface has 4-bit data bus.
It will be another story if the SDIO interface has 1-bit data bus only. in such case 0.2MB/s is reasonable.
2022-05-26 8:14 AM
Thanks for your message.
I confirm you that SDIO has 4-bit data bus (SDIO 3.0 at 1.8V with clk@25MHz) but the bit rate, at the moment, remains at 0.15-0.20MB/s using netconn API (I'm using multitasking environment).
Don't you think that LWIP can reach 2.0-3.0MB/s?
In this case should I use another TCP/IP stack? (for example FreeRTOS+TCP/IP)
Regards
2022-05-26 10:10 AM
The "Lw" in "LwIP" stands for "Light-weight" - it is not intended to be a high-performance stack...
2022-05-26 6:41 PM
I am not sure if 2.0-3.0MB/s is achievable, for either LwIP or FreeRTOS+TCP/IP.
anyway you need to get 1MB/s first, as you can only get 0.2MB/s.
some works are needed, such as, checksum offloading, more buffers (possible for STM32H747 which has about 500kB RAM if I remember well), client to send request in queue way, proper network data size(1kB or more), and so on, to improve the network throughput.
2022-05-27 12:20 AM
Ok. LW I thought it was for low RAM and ROM footprint but it was able to reach better performance than 200kBps...
Do you know other high-performance TCP/IP stack for STM32H7xx? Even not for free?
Thanks
2022-05-27 1:45 AM
"LW I thought it was for low RAM and ROM footprint"
Indeed.
"Do you know other high-performance TCP/IP stack for STM32H7xx?"
Not off hand. Google is your friend.
(other internet search engines are available)
2022-05-27 2:01 AM
I was just asking you, if you had used other TCP/IP stack for high-performance because you seemed prepared.
2022-05-27 2:10 AM
indeed. just confirming that I don't know - and not just ignoring you.
2022-05-27 2:28 AM
commercial version TCP/IP stack should be available for STM32H7, I believe.
I suppose you had better contact your local ST FAE/sales to get accurate information and support, regarding non-free stack.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.