2019-04-02 12:29 AM
Hi,
Want to be able to flash the target device( an STM32F446) using a propritary CAN interface. EI not use the bootloader default CAN flashing method.
As i understand it I must first make a IAP binary and flash using the bootloader by SWD. To then add the application I MUST use the IAP interface over CAN.
Is this correct?
Or is there a method to flash both IAP and application over SWD at the same time? And have them both in the same project in Atollic?
Also can I do a adress jump to the IAP from the application?
Hope anyone can give me some pointers.
Solved! Go to Solution.
2019-04-02 10:11 PM
Thank you both for the pointers.
I found this presentation at Atollic: http://info.atollic.com/hubfs/Whitepapers/Atollic_Develop_Debug_BootloaderApps_ARMCortex.pdf
That describe how to setup bootloader and application in the trueStudio and how to flash/debug using SWD.
2019-04-02 4:08 AM
You should be able to combine binaries into a singular monolithic image, or merge hex files.
The processor can jump to any location you tell it, in C consider function pointers.
2019-04-02 5:34 AM
Are you using the GNU toolchain? You should be able to create a padded binary for your bootloader (use the --pad-to address command line option for objcopy when generating a binary from the ELF), then just combine the bootloader binary and the application binary using "cat" or your favorite method of combining files.
For hex, I remember using a tool named Hexmate for joining Intel hex files. If you are on Linux, srec_cat will do the job too.
2019-04-02 10:11 PM
Thank you both for the pointers.
I found this presentation at Atollic: http://info.atollic.com/hubfs/Whitepapers/Atollic_Develop_Debug_BootloaderApps_ARMCortex.pdf
That describe how to setup bootloader and application in the trueStudio and how to flash/debug using SWD.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.