2025-02-10 7:35 AM - edited 2025-02-10 7:47 AM
Hi,
I am trying to setup an USB HS CDC example with NUCLEO-H7S3L8.
After setting up the projects for both CDC_Standalone and NUCLEO-H7S3L8 board example (for the latter I manually enabled the USB HS Device from CubeMX), I successfully ran each example to run from the external OSPI memory connected to the XSPI2 port.
STM32CubeMX standalone version is 6.13.0, while STM32CubeIDE version is 1.17.0.
STM32H7RS package version is the STM32Cube_FW_H7RS_V1.1.0.
1) I understand that setting up the CDC_Standalone example should result in a working example, but it does not.
2) The USPD interface is an TCPP03-M20, the BSP included in the board example (not the CDC_Standalone example) comes with a driver for this device which I understand it is automatically used by quickly looking at the code, but it seems it is not working neither.
"Not working" means that the USB device is not detected from the PC.
So for both cases, the function USBPD_DPM_Run() called into the main while loop hangs the execution of the firmware.
Is this behavior a known issue?
Is it needed some manual modification I am not aware of?
Thanks in advance for any hint.
s.
EDIT: I have attached the ioc file I am using.
2025-06-03 12:22 AM
Hello @FBL,
I did not test the github example. Of course the github example is not the same as the one provided within STM32CubeMX, since the project was created using the tool with the downloaded firmware from the tool, and the project did not have the tcpp203 and other dependencies linked in.
ST should review its software strategies.
Regards,
Simon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.