2020-03-19 1:43 AM
Let me tell you few things.
1: I have successfully connected my micro-controller (STM32F103C8T6) as HID device. I made 3 HID devices namely mouse, custom Keyboard and Point of Scale aka POS.
and they are working perfectly on Windows and Linux environment.
2: Now i want to connect them with my STM Discovery Board( STM32F407VG ) which is working as USB HOST.
3: I am using CubeMx IDE to generate code. Where i selected as USB HOST only and HID class. which by default give me two HID (mouse and Keyboard) API's for working. So I choose Mouse to see that Am i receiving data from mouse or not. and I successfully receiving data.
So what is my problem.
I want to understand that how this reports are coming to me. So later I can use them to see POS reports. Which API will give Endpoint data to me.
4: How can i get Report descriptor of printer class ?
#USB #POS #HID #HOST
2020-06-04 11:23 PM
I have solved my problems. Although there are many questions still there which will resolve slowly.
Now I have tested my code over 4 different type of printers including Dot Printer and Laser printer. All are working as expected.
Now I can announce that I have made my first printer class USB Host Driver using HAL library.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.