2024-07-17 12:46 AM
Hello@STTwo-32 @Remi QUINTIN ,
We are using STM32WB55RG MCU for our development. From the examples I came to know that the BLE device initially starts advertising as peripheral and the mobile device as central will be able to scan the device and initiate the connection. Once connected the device advertising is stopped.
But, I came through the BLE stack document and find out it is possible to have simultaneous connections with the BLE peripheral device upto 8.
I have been trying to have multiple connections of the BLE, like I want the device to be connected as well as advertiser so that it is possible to connect to with other central devices.
Do we have any examples in the STM32WB SDK which shows this behavior of connecting with multiple devices?
If yes, please let me know.
I have tried my side, changing few lines of code in the software as shown below
Firstly, In app_conf.h, i changed maximum number of simultaneous connections that the device will support to 8
#define CFG_BLE_NUM_LINK 8
Secondly, for advertising we use the function Adv_Request, which starts the advertising of the device.
static void Adv_Request(APP_BLE_ConnStatus_t NewStatus)
{
tBleStatus ret = BLE_STATUS_INVALID_PARAMS;
BleApplicationContext.Device_Connection_Status = NewStatus;
/* Start Fast or Low Power Advertising */
ret = aci_gap_set_discoverable(ADV_TYPE,
CFG_FAST_CONN_ADV_INTERVAL_MIN,
CFG_FAST_CONN_ADV_INTERVAL_MAX,
CFG_BLE_ADDRESS_TYPE,
ADV_FILTER,
sizeof(a_LocalName),
(uint8_t*) &a_LocalName,
BleApplicationContext.BleApplicationContext_legacy.advtServUUIDlen,
BleApplicationContext.BleApplicationContext_legacy.advtServUUID,
0,
0);
if (ret != BLE_STATUS_SUCCESS)
{
APP_DBG_MSG("==>> aci_gap_set_discoverable - fail, result: 0x%x \n", ret);
}
else
{
APP_DBG_MSG("==>> aci_gap_set_discoverable - Success\n");
}
/* USER CODE BEGIN Adv_Request_1*/
/* USER CODE END Adv_Request_1*/
/* Update Advertising data */
ret = aci_gap_update_adv_data(sizeof(a_ManufData), (uint8_t*) a_ManufData);
if (ret != BLE_STATUS_SUCCESS)
{
APP_DBG_MSG("==>> Start Fast Advertising Failed , result: %d \n\r", ret);
}
else
{
APP_DBG_MSG("==>> Success: Start Fast Advertising \n\r");
}
return;
}
After connection, How do we re-trigger this adv_request function, so that it is possible for the device to start advertising parallel while connected ?
Please let me know, the possible solutions for this task
Solved! Go to Solution.
2024-07-19 12:13 AM
Hello
Please have a look at the BLE_p2pRouteur project under the directory
STM32Cube_FW_WB_V1.20.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE
>>How to use Multipoint communication using BLE.
STM32WB55xx maintains seven simultaneously connections to transfer information from one device to an another remote.
Smartphone application is connected to one STM32WB55xx P2P router device allowing the control of six others
STM32WB55xx P2P Server devices (End Devices).
<<
2024-07-19 12:13 AM
Hello
Please have a look at the BLE_p2pRouteur project under the directory
STM32Cube_FW_WB_V1.20.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE
>>How to use Multipoint communication using BLE.
STM32WB55xx maintains seven simultaneously connections to transfer information from one device to an another remote.
Smartphone application is connected to one STM32WB55xx P2P router device allowing the control of six others
STM32WB55xx P2P Server devices (End Devices).
<<
2025-04-16 5:26 AM
Hi,
Are you now able to use STM32 as Central and connect with 5 simultaneous sensors.
If yes, please let me know
2025-04-23 5:33 AM
I dont get the difference regarding this use case versus what was described/confirmed a year ago.
One STM32WB55xx P2P central client is able to connect and control six others
STM32WB55xx P2P Server devices (End Devices = Peripherals) than can be sensors.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.